Part Number: BQ51003 Hello,
I am designing a Qi wireless power receiver using the BQ51003YFPR with the TDK WR222230-26M8-G coil (27 µH, DCR 1.1 ohm max, 22 mm diameter, rated 2W). TDK's datasheet for this coil lists BQ51003 as the reference IC, so I…
Part Number: BQ51003 Hello Support team.
We are planning to surface‑mount the BQ51003.
Could you provide the recommended temperature profile
and the allowable number of reflow cycles?
Part Number: BQ51003 Tool/software: we are using BQ51003 IC for wireless charging on my device. In the Qi9WPC) specification, I'd like to the specification of temperature while the device is on charging via wireless mothode, Qi.
Part Number: BQ51003 Hi,
Regarding to the post related to "BQ51003: No power transfert when strong coupling just high voltage large pulses for VRECT.", I have changed the communication capacitors for 4.7 nF, 6.2nF, 8.2nF and 10 nF. Initialy the communication…
Part Number: BQ51003 Tool/software: Hello,
We're considering a new design with BQ51003. Where can we purchase the transmitter to calibrate FOD?
I noticed people are getting answered in PM; is it some secret information?
Part Number: BQ51003 Hi Team
could you help on this SCH review?
WLC_BQ51003_2.pdf
the SCH refer below attached file.
TIDRIR7.PDF
it's a earphone project and this is for the box in the earphone. we hope it can support Qi wireless charge…
Part Number: BQ51003 Tool/software: Dear TI ,
I want to use the Texas Instrument "Wireless Power Receiver" in the main device which is Bluetooth based FDA certified Medical class 1 device and "Wireless Power Transmitter" for the wireless charger which…
Part Number: BQ51003 Other Parts Discussed in Thread: TIDA-00318 , Tool/software: Hi! Was checking out the schematics of the TIDA-00318 reference designs, and it caught my eye that there is a 20K resistors between RECT and FOD of BQ51003.
I checked…
Part Number: BQ51003 Tool/software: Trying to calibrate R_FOD on a new system using the BQ51003 Qi receiver. The Avid transmitter referenced in the documentation is no longer available with Avnet(?). All other posts in this forum seem to show a private…
Part Number: BQ51003 Tool/software: Good afternoon, I am using bq51003 for a wireless Qi charger receiver. I currently use a NTC as thermal protection, but I would like to replace it by a thermocouple so it is easier to set at different places. Has anyone…