Part Number: BQ51021 How is the variable output voltage attained on the BQ51021? Is it through a linear regulator (obviously built into the device)? Or is it by some other means? We're thinking about using it on a heat constrained device, but if the regulation…
Part Number: BQ51021 Other Parts Discussed in Thread: BQ51013B Hi,
I want to use bq51021 as receiver side IC in our project. Before implementing the project i have to do some testings. so I am trying to design a PCB which taken the pins out as male…
Part Number: BQ51021 Hi there,
we're evaluating the BQ51021 for a wireless power RX application utilizing the NTC temperature sense function. In principle, the circuit shows the expected behaviour (a TS pulse, width ~64ms, on the TS/CTRL pin appearing…
Hi bill,
Actually I'm a student and I not going to make any commercial products yet. I just built this as my final year project.It going to be demonstrate using a phantom module and I'm not going risk any life.
Best regards,
Kasun
University of…
Where can I find information about Kilim.
I found a document for programming, Quite big actually
Then I downloaded it. I could not open it.
Where can I find information to open my document.
Other Parts Discussed in Thread: BQ51021 Please let me know about bq51021 (see below).
--------------------------------------------------------------
①If battery doesn't connect to output (open), What happens?
Case 1:it isn't connected from first…
Other Parts Discussed in Thread: BQ51021 , BQ51020 Please let me know about bq51020 & bq51021 (see below).
・bq51020
Does bq51020 have the way to confirm the power loss and the other status?
・bq51021
I think the way to confirm the packet ID from…
Benjamin,
This is not a simple yes / no answer. The bq51021 can send up to 4 bytes of data as proprietary packets using registers 0xF1, 0xF2, 0xF3 and 0xF4 (refer to the datasheet for those registers). But, it's not as simple as putting data in the…
Part Number: BQ51020 Other Parts Discussed in Thread: BQ51021 , Greetings,
The latest BQ 51020 specification has on statement that is confusing. Section 8.3.5 is clear on how EN1/EN2 pins are used. However, the Pin Function table on page 3 describes…