Part Number: BQ51050B Other Parts Discussed in Thread: BQ51052B Hello,
I'm currently using BQ51050B to charge the battery of a device. The charge seems effective, unfortunately, the end of charge is never reach, even with charging current way lower…
Part Number: BQ51052B what is the maximum voltage between GND and Ac1 and GND and AC2?
to charge up to 300-500 ma what kind of inductor do you suggest (wurth elektronics part number)
thanks a lot and best regards
Part Number: BQ51052B I need to use BQ51052B devices in ATEX portable tools, do you have any application or suggestion to use it?
Thanks a lot and best regards
Andrea Brambati
Part Number: BQ51052B Other Parts Discussed in Thread: BQ500212 , I try to use BQ51052B and BQ500212 wirless charging systems.
I do not need to place "QI" label on my system, i ask if is necessary to join to WPC consortium.
Thanks a lot and best…
Part Number: BQ51052B 1: by using a NTC of 10K at 25° with B3977 can you help me to calculate the R1 and R3 value for charge between 0 to 45°
2: max charge current 300ma and 30 ma end of charge current, by using the data formula i 'd calculate…
Part Number: BQ51052B Dear,
I want to use the BQ51052B in a device, having a single Li-Ion cell, to be wireless charged on a standard Qi-charger. The BQ51052B should be Qi WPC compliant. So is my assumption correct that a BQ51052B based receiver can be…
Other Parts Discussed in Thread: BQ51052B , BQ25100H , BQ51003 hello,
I would like to know if it's possible to use BQ51052B to charge a battery Li-Po (120mAh).
already thank you for your answer.
Part Number: BQ51222 Other Parts Discussed in Thread: BQ51003 , BQ51020 , BQ25170 , BQ51221 , TIDA-00243 Hello,
I read the user manual about dimensioning RFOD and understand, that this has to be checked on the final product with a calibrated transmitter and…
Hi Rolf,
We do not guarantee operation or efficiency beyond the datasheet. The figures you are referring to pertain to the BQ51052B are showing efficiency in fast charge vs taper charge.
Part Number: BQ51013B Other Parts Discussed in Thread: BQ24076 , BQ51052B , , BQ51013
Hello,
Can someone from TI applications please take a look at the attached schematic? It's devoid of any proprietary information. It's a wireless charging + fuel gauge…