Part Number: BQ76905 Other Parts Discussed in Thread: MSPM0G3518 Hi,
Customer have reported below observations with BQ76905.
The AFE BQ76905 we are interfacing with MSPM0G3518 MCU I2C communication. Our HW design is for 4S so we are able to read…
Part Number: BQ76905 Other Parts Discussed in Thread: BQ76907-Q1 Dear,
What are the main differences between the two devices ( BQ76905 vs BQ76907-Q1) , besides the automotive version and the maximum Vbatt value?
Thanks
Part Number: BQ76905 Hi everyone,
I am designing a 5S BMS circuit using the BQ76905 IC. In my design, B+ is connected directly to the load via a cable. The PCB only has B- and P - outputs. Additionally, there is a connector for the cell sense wires…
Part Number: BQ76905
Hello TI Support Team,
I'm designing a 2S Li-Ion battery protection circuit using the BQ76905 paired with an ESP32 host MCU.
VC4A‒VC4B, VC4B‒VC3A, VC3A‒VC3B, VC3B‒VC2, VC2‒VC1 are the shorted connections as per the datasheet…
Part Number: BQ76905 Other Parts Discussed in Thread: TPS25730 , BQ25750 , , BQ25756 , BQ24650
Hello,
for the design of a mobile device powered by two LiFePO4 cells that can be charged via USB-C, I plan to use the following IC combinations:
- TPS25730…
Part Number: BQ76905 Other Parts Discussed in Thread: UCC27444 Hi Team,
We are using the BQ76905 to control the CHG and DSG pins, which then drive the MOSFETs through the UCC27444 gate-driver IC. Our design includes 14 charge MOSFETs and 14 discharge…
Part Number: BQ76905 Tool/software: Hi TI team,
Currently i am using BQ76905 BMS IC for one of my project with host mcu STM32H523RCT6. I want to use the CRC mode for communication. But it is not working when send the CRC byte then i get NACK. I think…
Part Number: BQ76905 Other Parts Discussed in Thread: ISO1540
Hello, I am having a lot of trouble gettting my design to work. Whartever I do, the BQ76905 stays unresponsive to any I2C message I am trying to send to it from the ESP32 microcontroller…
Part Number: BQ76905 Other Parts Discussed in Thread: BQ24640 , , BQ33100 Hi,
I would like to use BQ24640 for charge/discharge control of 4s supercapacitor. But I think I need another IC to monitor cell balance of multi-cell supercapacitor.
I am considering…
Part Number: BQ76905 Other Parts Discussed in Thread: MSPM0G3518
The AFE BQ76905 we are interfacing with MSPM0G3518 MCU I2C communication. Our HW design is for 4S so we are able to read/write the following parameters from AFE:
Read Individual Cell…