Part Number: BQ76905 Other Parts Discussed in Thread: BQ25750 , Tool/software: Hello,
Is there a linux driver and/or example code available for the BQ75905 battery monitor and the BQ25750 battery charge controller?
Thanks,
Brian
Part Number: BQ76905 We would like to have a method other than I2C for resetting the BQ76905. We are considering a single pole double throw switch that will disconnect Vbat and connect it to VSS through a resistor. Do you see any issues with Vbat being…
Part Number: BQ76905
Hi Team,
Posting on behalf of our customer.
We are using the BQ76905 in our design, connected to a 2-cell LiPo battery (2 × 4.2 V = 8.4 V total). The connection follows the typical configuration from the datasheet: VC5–VC4A…
Part Number: BQ76905 Tool/software: Hello,
I am trying to establish communication via I2C with the BQ76905 and the STM32L5xx Series. I have initalised the I2C1 line via CubeMX and am now trying to read cell voltages from the IC. I am using the functions…
Part Number: BQ76905 Hello team,
Is BQ76905 able to configured to output alert from an individual pin when overcurrent event occurs? This setting must be required in customer system.
Best regards,
Shotaro
Part Number: BQ76905 Hello, The I2C clock input (SCL) has rise/fall time requirements.
This input should be a schmitt trigger input so I don't understand why this input has rise/fall time requirements.
Could you explain?
Does this requirement really…
Part Number: BQ76905 Other Parts Discussed in Thread: BQ25792 Hello,
I am currently designing a 2S2P Li-ion battery pack using the BQ76905.
I have now completed the schematic, and before moving to routing I would really appreciate a schematic review…
Part Number: BQ76905 Hello!
I want to bring-up BQ76905 and read out PASSQ register and have difficulties as I did not find the process described in DS / TRM or SW manual or in code example.
I tried reading sub-command address + offset but…
Part Number: BQ76905 Tool/software: Hello,
I'm in the design process of a self contained system that is using 2S cells and integrating BQ76905 for protection and management.
I'm having a little trouble with where to GND the application part of the…