Part Number: BQ76907-Q1-DESIGN Other Parts Discussed in Thread: BQ76907 I want to read the DEVICE_NUMBER first. Below are my code and I2C waveforms. The BQ76907 is not sending response data.
void Subcommands(uint16_t command, uint16_t data, uint8_t…
Part Number: BQ76907-Q1 Dears,
Put the voltage of one battery artificially at 0v, and the voltage of other batteries is 2.6v normally. If charging is not started, an equalization instruction is given to the normal battery, and it is found that it…
Part Number: BQ76907-Q1 Other Parts Discussed in Thread: BQ76907 Dear Team,
A customer is using the BQ76907 for supercapacitor charge management. Currently, regarding the BQ76907 chip, we have the following questions and would appreciate your confirmation…
Part Number: BQ76907-Q1 Other Parts Discussed in Thread: BQ76907 Hi, Team
one of my key customer, KyungShin is asking question on BQ76907.
Please note customer is trying to design that BAT pin is supplied from external 12V, not Cell.
※ The reason…
Part Number: BQ76907-Q1 Other Parts Discussed in Thread: BQ76907 Dears,
The customer is using the BQ76907 to design a supercapacitor charging management system. They need to obtain the amount of charge during capacitor discharge. Using the reference…
Part Number: BQ76907 Hello TI team,
I am considering using the BQ76907 as the BMS AFE IC for a new design. In this application, the device will only be used for voltage and current monitoring.
However, due to mechanical design constraints, the connector…
Part Number: BQ76907 Dear Texas Instruments Support Team,
I am currently developing a Battery Management System using the BQ76907 device interfaced with an STM32F407 microcontroller. I am using custom firmware with I2C communication to configure and…
Part Number: BQ76907-Q1 Other Parts Discussed in Thread: BQ76907 Hi TI team,
I would like to confirm whether our 4-cell battery configuration is correct when using the BQ76907.
In our design:
A 4-series cell stack (4S) is used
Could you please…
Part Number: BQ76907-Q1 Hi Team,
In the figure below, these two FETs act as switches to ground; one is responsible for discharging, and the other for charging. The FET control is configured in automatic mode.
Question 1: When the voltage equalization…
Part Number: BQ76907 Hello TI Support Team,
I am working with the BQ76907 IC and currently facing an issue while reading temperature from the TS pin using an external NTC thermistor.
Setup details:
IC: BQ76907
Thermistor: 1k NTC
…