Hi Hasan,
Regarding the bq76200, measuring the gate to ground could be pulling down the voltage at the gate. The charge pump is not very strong, and we've seen cases where a probe can pull the voltage down. It would be better to measure the gate to source…
Part Number: BQ76930 Hello TI Team.
Does bq76930(bq769x0) have reference flow chart diagram for better inside of the protection setting? As it has shown below for voltage protection.
Part Number: BQ76930 Hi
I have a query need your help.
The 16-bit CC also completes an update every 250ms in ALWAYS ON mode. How many times are the currents sampled?
What is the sampling rate? What algorithm was used? How to ensure the correctness of…
Part Number: BQ76930 Other Parts Discussed in Thread: BQ76942 , BQSTUDIO Hi ,
Hello, I would like to ask.
I recently need to program the BQ76930 IC, but I want to simulate I2C myself to communicate with the IC to complete the programming.
I would like…
Part Number: BQ76930 Other Parts Discussed in Thread: BQ78350 , BQ76200 , , BQ76952 , BQ34Z100 Hi,
We are looking for suitable chipset to support 9S1P LiFEPO4 battery pack for Industrial applications.
Below are the major requirements.
* Charge/discharge control…
Part Number: BQ76930 Other Parts Discussed in Thread: BQ76940 , I am using a 25s Battery Pack for the first 15 cells i use BQ76940 IC and for the remaining 10 cells I use BQ76930 IC but Now I see that my 10 cells are discharging faster than the first 15…
Part Number: BQ76930 We have a new BMS design based on the BQ76930 where we have serious noisy measurements on the CC ADC voltage; at rest with no current flowing through the shunt we measure approx 400mV top-top noise. Shortingthe differential input…
Part Number: BQ76930 Hi E2E,
We had a problem with the IC's temperature detection function.
In the design, we connected the TS1 to an external thermistor to detect the temperature, and the VC5x connected a fixed 10kΩ to the TS2.
1, if TEMP_SEL…