Part Number: BQ76952 Hi
I have a query need your help. Thermistor coefficient calculate fail, and the failure figure as below.
Attached the zip file.
4265.Temp1.zip 103F3435 28# 100线长 230523 (1).pdf
Please help check it.
Thanks
Star
Part Number: BQ27220 Hi experts,
I think that the unit of the temperature value by the external thermistor is 0.1K° in the datasheet, but when using other thermistors, are there any parameters that need to be changed in the BQ27220?
My customer is…
Hello Jason,
To get the best accuracy, you will want to calibrate it.
You should put the thermistor resistance vs. temperature on our BQ769X2-THERMISTOR-COEFF-CALCULATOR coefficient calculator. Using these coefficients will provide the best accuracy. Can…
Hello Ankur, 1. Please refer to this: BQ769x2 Thermistor Coefficient Calculator . This BQ769x2 Thermistor Coefficient Calculator Tool FAQ may also be useful. 2. The input should be in Ohms. Best Regards, Alexis
Hello Enrico, We don’t have a production tool for the BQ769142, however, we have the BQ769x2 Software Development Guide , a BQ769x2 Thermistor Co-eff-Calculator tool, and BQStudio for software tools.
I'm looping in another engineer to answer your…
Part Number: BQ76952 Other Parts Discussed in Thread: BQ34Z100-G1 , TIDA-010030 , BQ76920 , BQ76930 , BQ78350-R1A , BQ76940 Do the BQ769x2 family of device have the capability to do gauging?
Hi Kish,
You should be able to configure the multipurpose pins to be compatible with thermistor measurements. Did you follow all the steps listed in this FAQ? [FAQ] BQ76952: How to configure a multipurpose pin to work as a thermistor in the BQ769x2 family…
Part Number: BQ76952 Other Parts Discussed in Thread: TIDA-010208 , BQSTUDIO Hi TI expert,
we have tested the thermal measurement and find that the temperature error is much bigger after change the Coef parameters in the data memory.
I have re-calculate…
Hi Fabio,
You mentioned that the customer has not done any temperature calibration. Has the customer used the BQ769x2 thermistor coefficient calculator to update the coefficients for the thermistor they selected? The tool and instructions are located here…
Part Number: BQ34110 i want to know the required Ext Coeffs values for that sensor NTCG163JX103DTDS
its data from datasheet :
Resistance [25c] : 10000
resistance tolerance = + or - 0.5%
B constant [25/50 c] = 3380 k
B constant [25/75 c] = 3422 k
B constant…