Part Number: BQ76PL455EVM I am developing algorithm for the Battery Management System using BQ76PL455-EVM and STM32F407 MCU. I have configured the UART as defined below:
1) Baudrate: 250K
2) Word Length : 8 bit
3) Parity bit: None
4) Stop bit: 1
I have…
Other Parts Discussed in Thread: BQ79616EVM-021 , BQ76PL455EVM , BQ79616 , BQ76PL455A Hello TI Support,
1. I would like to know how to connect BQ79616EVM-021 with TMS570LC43x LaunchPad. Do I just need to connect UART for them? Or, do I still need any adapter…
Part Number: LAUNCHXL2-TMS57012 Other Parts Discussed in Thread: BQ76PL455EVM , HALCOGEN I have currently on a BMS project using LAUNCHXL2-TMS57012 as controller and BQ76PL455EVM as battery sensing.
I have successfully communicate with BQ76PL455EVM/BQ79616EVM…
Part Number: BQ76PL455EVM Hello,
1- I have a bq76PL455EVM. It connects with microcontroller. At the first power-up, the D22 led seems to turn on as soon as the Wake signal is gone, but it flickers and the EVM does not wake up. I connect BAT16 and BAT0…
Part Number: BQ76PL455EVM Other Parts Discussed in Thread: TMS570LS1224 Hi,
I am using TMS570LS12 launchpad (it has TMS570LS1224 controller) with bq76pl455evm. I have connected EVM with 16 cells and I am unable to communicate and read any response from…
Part Number: BQ76PL455EVM Other Parts Discussed in Thread: TMS570LS1224 , HALCOGEN Hi,
I am using TMS570LS12 launchpad (it has TMS570LS1224 controller) with bq76pl455evm. i have connected EVM with 16 cells and I am unable to communicate and read any response…
Part Number: BQ76PL455EVM Hi Team,
I have connected battery pack to BQ EVM. I am not able to read correct voltage of cell1, after debugging I found that there is 70mv of difference between BAT0 and BAT0S. Also resistance between these two points was…
This is my all code
/**
*
* @file main.c
* @brief this file contains example command sequences and functions to interface with the bq76PL455A-Q1 from a
* microcontroller. The examples provided are described in the bq76PL455A-Q1 Software Design…
Part Number: BQ76PL455EVM Hello Sir/Madam,
I am using bq76PL455EVM. I reviewed the code that TI wrote for the TMS570 MCU. I noticed that Real Time Interrupt is used. If I'm not mistaken it means something to do with RTOS. And my problem is I don't have…
Part Number: BQ76PL455EVM Hi,
1) Which microcontroller has been used on BQ76PL455EVM?
2) Is there any provision for by passing this controller? I want to connect my own controller to BQ76PL455EVM is it possible? if yes then How?
Regards,
Aniket.