Hi Carl,
I encourage you once again to consider BQ79616-Q1 for your design as we don't recommend BQ76PL536 for new designs- please see the below message posted on BQ76PL536's product page for reference.
Best Regards,
Julia Louis
Part Number: BQ76PL536 Tool/software: Code Composer Studio Hi all!
I designed a pcb project with BQ76PL536 .And now , its time to code! But I have a problem. I want to find the example code project for MS430 . Can anyone share with me a link? I searched…
Part Number: BQ79616 Other Parts Discussed in Thread: TIDA-010271 , BQ76PL536 Hello I want to design a bms with bq79616 cell monitor-balancer for 16 cells. I can access the design files with TIDA-010271. I want to use active balancing, but I think the chip…
Part Number: BQ76PL536 Hello
i am use bq76PL536 evm3 in my project. i want to use STM32 mcu and need some code for starting my project. i read TI example for MSP430 MCU's , but that a bit complicated for me!
please guidance me or if it's possible share…
Part Number: BQ76PL536 My customer has made design using the Industrial A-Version. One option to fix a delivery issue could be the usage of the old version "none-A". Which differences need to be checked to use BQ76PL536PAP in a BQ76PL536APAP socket. Thanks…
Part Number: BQ76PL536 Hi,
When testing the battery balance with the computer on the official website based on BQ76pl536 EVM, the voltage only drops by 0.1V after opening the balance.
I want to know how to set the equilibrium value, so that the balance…
Part Number: BQ76PL536A Other Parts Discussed in Thread: BQ76PL536 Hi All,
Nice to meet you in E2E. I have encountered a sleep issue of BQ76PL536.
Customer has manipulated IO_Control and Alter bit. But the base 536 still consume 400uA, while the top 2…
Part Number: BQ76PL536 Hello,
In my application, only one BQ76PL536 is connected to DSP28035, so it works as device to host mode.
I didn't change the address for BQ76PL536, so the address is 0, and the clock frequency was 250kHz.
I capture…
Part Number: BQ76PL536 Hi,
I would like to use the BQ76PL536 IC. I see you can connect 6 cells in series.
If our pack has 6 cells in series and 3 in parallel, do we need to use 3 IC's for all 18 cells?
Or can we chain the parallel cells to just one…
Part Number: BQ76PL536
Hi,
I'm working on battery management system for my 6 cells and i want to drive the mosfet in 100Khz frequency.
So can CBn output of the BQ76PL536 drive in this frequency, if not can i have an idea what is the maximum switching…