Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: BQ77PL900 Dear colleagues,
Could you please help me to read BQ77PL900 datasheet? :)
It stands that CBEN bit is set to 0 by default, which disables cell balancing. But if we want to work in pure stand-alone mode, without any host controller…
Part Number: BQ77PL900 Hello guys, I'm trying to build a BMS, using the IC BQ77PL900 and the FETs that I already have here at college. I thought this was the best IC to be used since it has the EVM that I can take as a basis for construction. However…
Part Number: BQ77PL900 Hello.
I can not find out recommend Land Pattern of BQ77PL900.
Package model is DL(R-PDSO-G48).
Could you teach me that,please ?
Thank for the Support.
Regards,
Part Number: LM5171-Q1 Other Parts Discussed in Thread: LM5171 , BQ77PL900 , BQ78PL114 I plan to connect two 600 watt 3 volt Sodium Ion Battery Cells in Series Parallel and plan to use the LM5171 + bq77PL900 for passive cell balancing bq78PL114. Please keep…
Part Number: BQ77PL900 Other Parts Discussed in Thread: BQ77915 , BQ76930 , BQ77905 Hi,
Can anyone tell me what's the best way to monitor the temperature for a 6S3P battery pack? I'm using the bq77PL900 to monitor and balance the cells but there…
Feng Ji I would need to combine a passive cell balancer bq77PL900 or a active cell balancer bq78PL114. Please keep in mind we want these components to 8000-10,000 Battery Cycles over 20-25 years. By following your advice by combining two 3 volts sodium…
Part Number: BQ77PL900EVM-001 Hello,
I am having issues with getting the BQ77PL900 EVM to connect to the evaluation software. I am using the EV2400, which should work with the BQ77PL900 (this is stated in the EVM user guide). However, when I run the…
Part Number: BQ77PL900 Is there documentation on the bits in the EEPROM register 0x0b? This will help clear up confusion about programming.This is related to writing a production friendly script for programming the bq77PL900.
The text in the EEPROM Write…
Part Number: BQ77PL900 Hi Ti.
I have some questions about BQ77PL900's cell balancing operation.
Please let me know.
1. I already knew cell balancing is operated in VOV ~ (VOV – ΔVOVH), But when discharging, cell balancing is not working?…
Part Number: LM5171-Q1 Other Parts Discussed in Thread: LM5171 , , BQ77PL900 , BQ78PL114
The datasheet for the LM5171 Evaluation Module says 6 volts, but the LM5171-Q1 MOSFET chips say
Wide input voltage range: 2.7 V to 36 V
Programmable output voltage…