Part Number: BQ78350-DEVICE-FW Other Parts Discussed in Thread: BQ78350 , BQSTUDIO Tool/software: Hello,
I have a .srec file from Battery Management Studio for BQ78350, I parse the .srec file. I can Unseal, Unseal-Full access the device and I can make…
Part Number: BQ78350-R1A Other Parts Discussed in Thread: BQ78350-R1
Dear TI,
Although we set the self-discharge value of our 10S2P battery to 0.88%, during our 60-hour sleep mode test the battery SOC level
Test Start point,
DUT screen capture…
Part Number: BQ78350-DEVICE-FW Tool/software: Dear TI,
Although we set the self-discharge value of our 10S2P battery to 0.88%, during our 60-hour sleep mode test the battery SOC level
Test Start point,
DUT screen capture after 60 hours,
…
Part Number: BQ78350-R1 Other Parts Discussed in Thread: BQSTUDIO Hello,
I am using BQ78350-R1.
After a qualified discharge, I see that DOD at EDV2 is learned incorrectly.
Battery Information:
10S2P
Design Capacity mAh:9000
Design Capacity…
Part Number: BQ78350-DEVICE-FW Tool/software: Hi E2E,
I am trying to download the BQ78350-R2-FW from the link below.
www.ti.com/.../R2-V2.02
But the download page shows 'Error 404'."
Please assist me in obtaining the "BQ78350-R2-FW".
Thanks…
Part Number: BQ78350-DEVICE-FW Other Parts Discussed in Thread: BQ76940 , BQ78350 , BQSTUDIO Tool/software: Hello,
I am commissioning a new BMS based on the reference design for the BQ78350 with the BQ76940 and BQ76200PWR, the only notable exception…
Part Number: BQ78350-DEVICE-FW Other Parts Discussed in Thread: BQ78350 Tool/software: Hello,
Until now I have worked with the bq78350_R2. Now I have switched to the R3 version to use the balancing at rest, but it does not work.
In the post
https…
Part Number: BQ78350-DEVICE-FW Other Parts Discussed in Thread: BQSTUDIO , BQ78350 Tool/software: Hello!
I have a problem with cell balancing at rest with bq78350R3. I have a 15S LiFePO4 battery where cell balacing at rest is necessary. * bqz Device…
Part Number: BQ78350-DEVICE-FW Tool/software: Hello Ti Team,
Our configuration file is attached. Battery FCC is 10000mAh and I am using ipsclae, so our real capacity is 100Ah.
I am using Fixed_EDV0. I noticed that DOD at EDV2 value decreases every…
Part Number: BQ78350-DEVICE-FW
Tool/software:
I also tried same test with my current is below quite current, but still rest mode is not triggered. how to enable cell balancing in rest mode. Here i also attached my configuration file for understanding…