Part Number: BQ27Z746 Hello,
Wondering if there is anyway to shutdown the GG via an I2C cmd with ENAB pin just constantly pulled to ground.
Thanks!
Austin
Part Number: BQ27Z561-R2-DEVICE-FW Other Parts Discussed in Thread: ADS1285EVM-PDK , ADS1285 I'm testing the ADS1285EVM-PDK 32bits ADC board, but I met some problems. When I only connect the UBS wire to PC and do not connect sonser, I measure the voltage…
Part Number: BQ78350-R2-DEVICE-FW Hi Matt,
Please can you tell us about status about the R3 release. We need them quite urgent now. :-)
Many thanks,
Dick
Part Number: BQ78350-R2-DEVICE-FW Hello Sir:
We have three questions about BQ78350-R2.
1. We want to know that the EC3-EC0 bits of batterystatus display 0x07, UnknownError.
What's the meaning? Why does the device have this message?
2. What conditions…
Part Number: BQ78350-R2-DEVICE-FW
Dear Sir/Madam,
I have a question about advance charge algorithm. Could you help me, please about this issue?
In the below picture shows temperature and current value for low and standart temperature. Does this mean…
Part Number: BQ78350-R2-DEVICE-FW Hi everybody,
I have got a problem with my bq78350_R2 and bqStudio. When trying to UNSEAL/UNSEAL_TO_FULL I get some problems.
When I try to UNSEAL it with the COMMAND Button - UNSEAL (with the correct key) it does not UNSEAL…
Part Number: BQ78350-DEVICE-FW
Hi,
We encounter bad balancing times on our BMS. All balancing parameters are met, but still the CB bit is often not active. It seems like the balancing algorithm only balances away a single high cell, but does not account…
Part Number: BQ78350-R2-DEVICE-FW Hi everyone,
I have a problem regarding unsealing.
I have one batterypack with a bq78350 + bq76940 which is unsealed. I tried reading the seal password from this device but somehow I am lost.
I also have 3 identical batterypacks…
Part Number: BQ78350-R2-DEVICE-FW The cell I use is actually given in CHEMID and I program it to BQ78350-R2.
But, my battery pack consists of multiple of those cells connected in series and also parallel.
As far as I could understand, the CHEMID for CEDV…