Part Number: BQ78350-R2-DEVICE-FW Other Parts Discussed in Thread: BQ78350
Dear Sir/Madam,
I have a question about advance charge algorithm. Could you help me, please about this issue?
In the below picture shows temperature and current value for low…
Part Number: BQ78350-R2-DEVICE-FW Other Parts Discussed in Thread: BQ78350 , BQSTUDIO Hi everybody,
I have got a problem with my bq78350_R2 and bqStudio. When trying to UNSEAL/UNSEAL_TO_FULL I get some problems.
When I try to UNSEAL it with the COMMAND Button…
Part Number: BQ78350-R2-DEVICE-FW Other Parts Discussed in Thread: BQ78350-R1 The cell I use is actually given in CHEMID and I program it to BQ78350-R2.
But, my battery pack consists of multiple of those cells connected in series and also parallel.
As…
Part Number: BQ78350-R2-DEVICE-FW Other Parts Discussed in Thread: BQ76940 , BQ78350 , BQ78350-R1 Hi everyone,
I have a problem regarding unsealing.
I have one batterypack with a bq78350 + bq76940 which is unsealed. I tried reading the seal password from…
Part Number: BQ78350-R2-DEVICE-FW Hi Matt,
Please can you tell us about status about the R3 release. We need them quite urgent now. :-)
Many thanks,
Dick
Part Number: BQ78350-R2-DEVICE-FW Other Parts Discussed in Thread: BQ78350 Hi,
Is there a 100AH (15series cell 43,5V-54,5V) cell chemistry suitable BQ78350R2? Cells are LiFePO4. Could you help me this issue?
Best Regards,
KT
Part Number: BQ78350-R2-DEVICE-FW Other Parts Discussed in Thread: BQ78350 In my application, especially for the high temperature range battery can go into Cell Over Temperature protection, disable the discharge and continue after recovering. Is it allowed…
Part Number: BQ78350-R2-DEVICE-FW I have to use VSCALE 10 (in order to use SAFE feature).
I may need to use IPSCALE 10 too.
When I submit the prepackage to GPC, am I supposed to send raw reported values by BQ78350-R2 (real values divided by 10) or actual…
Part Number: BQ78350-R2-DEVICE-FW Other Parts Discussed in Thread: BQ78350 , GPCCEDV , BQSTUDIO Hello,
We are using BQ79350-R1 IC with R2 firmware as Fuel Gauge to calculate our SOC. As suggested by the Guide for BQ78350, we have used GPC tool to calculate…