Part Number: BQ78Z100 Hello Sir/Ma'am,
We are planning to use the BQ78Z100 chip inside our battery pack, so its implementation says it can be used inside the battery pack.
But I just wanted to know that as our battery is intrinsically safe, so putting…
Part Number: BQ78Z100 To whom it may concern:
We are using BQ78Z100 on a single cell battery. The OCD is set to 2.6V, 2s. During the verification test, the delay is tested as 3.8s when 2.6A applied, and 3.5s when 2.7A applied. So could you help to check…
Part Number: BQ78Z100 Hello Sire Please refer below figure.
Left portion is coming from golden.gg, right portion is coming from product)
Our battery pack is one cell application.
But our life time cycle data got 6095mV and 127degree.
Can you give us some…
Part Number: BQ78Z100 Hello,
My name is Simeon Aleksandrov, I am an FAE intern at TI BeNeLux.
I was interested to know if the BQ78Z100 supports clock stretching when it is the slave device in an I2C link? I could not find anything in the specifications…
Part Number: BQ78Z100 Other Parts Discussed in Thread: GPCCHEM dear
customer use BQ78Z100 and upload chemial ID data and hope it can return relative data from belowwebsize which success in the pass few months
https://www.ti.com/powercalculator/docs/gpc/gpcUpload.ts…
Part Number: BQ78Z100 Dear Expert
For the BQ78Z100 2-string battery that we currently mass-produce, about 0.5% of the finished battery will trigger SOV protection after running the cycle. PF records that Cell1 and Cell1 Voltage have reached 5680mV, but…
Part Number: BQ78Z100 Other Parts Discussed in Thread: BQSTUDIO Hi,
Good Day. I have a customer who is working with BQ78Z100. Please see below his query for your reference. Thank you very much.
I would like to easily disable the charge and discharge…
Part Number: BQ78Z100 Hello Sir:
We are using BQ78z100 on our battery pack, but we has some seal questions on our battery pack.
We release 2 lots battery pack to customer side, one lot used default seal key, other one used our new seal key.
Cause some…
Part Number: BQ78Z100 Hi TI team,
We already use the BQ78Z100 in a 2-series cell configuration and now we are planning to use the same IC for a single cell configuration.
I don't find any datasheet recommends if the resistor/capacitor need to be removed…