Hello,
I am using isolator IC ISO1514 with both side pullup added on I2C lines.
I am using S DK example code " bq7690x_control_i2c" in that same code stuck in while loop for TX complete ( gI2cControllerStatus == I2C_STATUS_TX_INPROGRESS).
I didn…
Part Number: CC2652PSIP Tool/software: Hi Team,
We are promoting TI CC2652PSIP and one of customer need example code for multi-role to switch from the following three function: Peripheral / Beacon / Scan .
Please help to check if TI have the example…
Hi Daria,
MSPM0 support CRC16-CCITT and CRC32- ISO3309 polynomial functions, please see Chapter 22 CRC of MSPM0 G-Series 80-MHz Microcontrollers Technical Reference Manual (Rev. B) for more details.
Which CRC algorithm is customer desiring for ?
Best Regards…
Part Number: MSP430I2041 Other Parts Discussed in Thread: MSP430WARE Tool/software: Hello,
Do you have code example of SD24 Differential Input?
I check the MSP430ware but it have only single-input example.
And do you have example schematic for this usecase…
Part Number: TCAN1145-Q1 Tool/software: Hi,
I’m working with the TCAN1145-Q1 and would like to know if any reference code or example code is available for this device.
Thanks, Hong
Part Number: MCU-PLUS-SDK-AM263PX Tool/software: Hi,
I’m working with the AM263Px CC evaluation board and the AM263x controlCARD Dock. I tried to run the ADC example ‘ADC SOC Continuous’ from the SDK version mcu_plus_sdk_am263px_10_00_00_35. I feed the…
Other Parts Discussed in Thread: TIDA-010054 零件编号: TIDA-010054
工具/软件:
你好
我目前正在学习 TIDA-010054内容。我想知道 TI 官方是否提供了此参考设计的随附示例代码以供学习。如果是这样,您能帮我告诉我如何获得它吗?我将不胜感激!
Part Number: EK-TM4C123GXL Tool/software: I am having trouble seeing the I2C SDA and SCL signals on my EK-TM4C123GXL Launchpad using example code.
I have pins PB2 on CH1 and PB3 on CH2.
Both PB2 and PB3 are connected to 1.5k pull up resistors.
Below is…
Hi Darryl,
I am not sure whether you are still working on this project or not.
However recently i came across one issue and the solution for that issue also solved the problem for this issue.
Here is the reference issue & please refer my last comment…