Part Number: BQ79606A-Q1 I am trying to use the BQ79606a-Q1 EVM through the use of the GUI which is used to configure the evm..... i am not able to understand the balancing part of it say for eg: the duty cycle represents the balancing of each banks odd…
Part Number: BQ79606A-Q1 Dear Mr. Mrs.
About BQ79606 FMEDA calculate tool, we have some questions need your help:
“Life Cycle” in <Mission Profile Tailoring>. Our project’s life cycle is very special, it need 15 years but active operating…
Part Number: BQ79606A-Q1 I am trying to use the BQ79606 EVM for Li-ion cell monitoring, its said that this device is compatible with the TMS570 module. Is it possible to connect any other device like C2000 F28379D for monitoring the cells along with BQ…
Part Number: BQ79606A-Q1 Other Parts Discussed in Thread: BQ79606-Q1 , BQ79600-Q1 2つの質問があります。
質問1,BQ79606-Q1とBQ79600-Q1をDaisy Chain通信で使う場合、BQ79606-Q1の機能にて制限される機能がありますか?
質問2,リチュームイオン電池のセルを3直列で、使用できるAFE-ICは、BQ79606-Q1が一番 最新ですか?
Part Number: BQ79606A-Q1 Hello,
we observe a lot of BMS where one of 6 BQs on the BMS shows a UV comparator error even if the measured voltage is fine. The strange thing is, its always cell 6. The error appears directly after start up. Has someone an…
Part Number: BQ79606A-Q1 Dear all, we are developing an application that requires to access an spi eeprom through the bq79606 spi master function.
The problem is that no matter how we try the only think we succeeded in is to drive low and high the chip…
Part Number: BQ79606A-Q1 Hi team,
Interested application question for the BQ79606A-Q1. The BQ79606A-Q1 specifies a minimum of 3 cell voltage measurements.
Does it need to measure a minimum of 3 series-connected cells? or just three measurements?
In the…
Part Number: BQ79606A-Q1 Hi team,
My customer encountered hot plug issue recently. Communication failure or devices damage may occur when customer replaces the battery.
Customer’s SCH is attached, the questions is:
Customer said increasing the resistor…
Part Number: BQ79606A-Q1 Other Parts Discussed in Thread: BQ79616 Hello! I am working with a BQ79600 bridge IC and a stack of BQ79606A monitoring ICs.
I am trying to figure out the correct auto-addressing procedure. The datasheet for the BQ79600 lists an…