Part Number: BQ79614-Q1 Hello ! What is the applicable resistance range for the Rvc resistors of the BQ79614? We have encountered two failure cases of the 100 ohm Rvc resistors at the VC0 pin: their resistances rose to 300 ohm and 530 ohm respectively…
Part Number: BQ79614-Q1 I would like to confirm that this chip only supports passive cell balancing and is not capable of utilizing active cell balancing.
If this BQ does not support actice cell balancing, are there any other similar battery monitoring…
Other Parts Discussed in Thread: BQ79616-Q1 , BQ79614-Q1 , BQ79616
Dear TI Support Team,
For testing purposes, I am looking for a way to read all the registers of the BQ79614 in order to verify if any values have changed during runtime.
Is there…
Part Number: BQ79614-Q1 Other Parts Discussed in Thread: USB2ANY Hello,
We use the BQ79614-Q1 on a custom PCB in combination with the BQ79614EVM-021 (evaluation board). When sending wake-up ping through the BQAutoEval, the AVDD DVDD LDOIn Negative 5V…
Part Number: BQ79614-Q1 If the wake-up process of the BQ79614-Q1 chip is functioning correctly but auto addressing is failing, what could be the potential reasons for this issue?
With kind regards
Siva.
Part Number: BQ79614-Q1 If the wake-up process of the BQ79614-Q1 chip is functioning correctly but auto addressing is failing, what could be the potential reasons for this issue plz?
With kind regards
Siva
Part Number: BQ79614-Q1 Other Parts Discussed in Thread: BQ79616-Q1
I have connected 2 BQ79614-Q1 in daisy chain configuration. The COMH of the base device is connected via Capacitor Isolation to the COML of the 2nd device. COML of the base device is…
Part Number: BQ79614-Q1
Tool/software:
Hi,
Can you transfer us a schematic of the inputs VC0, VC1, ...
RC filter are present in front of these inputs.
At startup, we measure a current of 300mA during about few 100µsec threw the 100R resistor…
Part Number: BQ79614-Q1 Other Parts Discussed in Thread: USB2ANY
Hi,
I have a problem where communication is not working on my stack devices.
I had it working before but suddenly some stack modules are only listening to wake tone and then wont…
Hi Ben,
Benjamin Luty said: 1) Do you detect that the devices are waking up after the wake ping (with an increase in current draw)?
Yes, I can detect the devices are waking by probing AVDD, DVDD, and CVDD signals. The devices are waking correctly…