Part Number: BQ79616-Q1 Tool/software: Hi Experts,
For BQ79616-Q1, I only use the 16 cell VCx channels of BQ79616-Q1 and do not use its balanced VBx channels. How are the 16 balanced channels connected? Is it suspended or are they all connected to BAT…
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79616 Tool/software: Hey TI Experts,
We have developed our bms using bq79616 afe. The bq79616 is communicating directly over UART with a stm32 microcontroller. It is made sure all the hardware…
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79652-Q1 Hi,
Earlier, we have read the data of cell through daisy chain with the help bridge device. Now we want to move UART communication. So we have connect the UART port (PIN 52 & PIN 53…
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79616 Tool/software: Dears CC,
We have run the power supply BIST at start up in the BQ79616-Q1 device and found PWRBIST_Fail Bit =1.
We further diagnosed and checked all the bits from FAULT_PWR1…
Part Number: BQ79616-Q1
Tool/software:
I have a question about the accuracy of OV comparators. On page 16 of the datasheet, V OV_COMP_ACC is stated as ±24 to 28 mV, but when I checked it, there was an error of more than 100 mV.
Therefore, when cell…
Part Number: BQ79616-Q1 Tool/software: Hi,
This question is actually regarding BQ79718 , but it was not listed as a choice in "Part number" above.
When using BQ79718 in a ring configuration:
How will a "link cut" (a single comm. link between two…
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79616 , Tool/software: Hi All,
We have a schematic we'd like to have reviewed/get feedback on if at all possible. Mostly wanting to make sure we didn't miss anything obvious before sending it…
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79616 Dear TI expert,
I am designing new BMS, where i can download bq79616-Q1 Example Code 0.1 ?
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79616
Tool/software:
Hi TI Team,
My customer is willing to use an external EEPROM and control it via BQ79616's GPIOs in SPI master mode.
I saw a similar application mentioned in the…
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79616 Tool/software: Hi Team,
I am using two BQ79616 IC's in daisy chain, the communication between MCU and base IC is through level shift circuit using UART.
I am using a configuration for…