Part Number: BQ79631-Q1
Is there a defined behavior/ if reading back undefined registers from a BQ79631-Q1 device ?
e.g. if i read from adress 0x52D (FAULT_SUMMARY) with length 45(dezimal) to obtain all fault information in one read, i will read all…
Part Number: BQ79631-Q1 Hello,
We used GPIO(MAIN_ADC) for insulation detection and found that when the input voltage to GPIO8 is less than 0.045V, the data returned by channel 8 is always 0.045V(The number returned is 0X129), but when the voltage is…
Part Number: BQ79631-Q1 Hello, Regarding the open wire diagnostic of the SRN/SRP channels. If I turn on the OW Sink on SRN/SRP DIAG_COMP_CTRL3. OW_SNK[1:0] = 11, I expect the measured voltage to change in case of an open wire. If I try this out on a open…
Part Number: BQ79631-Q1 Tool/software: hello,
I am an engineer developing BMS in Korea. I would like to develop a product using TI's IC solutions.
BQ79631 I would like to purchase BQ79631EVM along with full datasheet, schematic and other related data…
Part Number: BQ79631-Q1 Hello,
I would like to purchase BQ79631EVM along with its complete datasheet, schematics, and other relevant data. On the product page for the BQ79631-Q1, it mentions a BQ79631 Evaluation Board, but I cannot find an order link…
Part Number: BQ79631-Q1 Hello TI team
How can we order the BQ79631EVM Evaluation Module?
We have already signed NDA, can you please support on this?
Thanks and regards, Ramchandra Bhosale.
Part Number: BQ79631-Q1
Dear TI Team,
We are working on adding BQ79631-Q1 chip in 500V Battery Management System for HV sense application of 500 V system.
We need to pass the AC voltage withstand test for the BMS.
In this test, 1800 V AC voltage, 50…
Part Number: BQ79631-Q1 Other Parts Discussed in Thread: USB2ANY , BQ79616-Q1 , , BQ79616 , TIDA-00792
Hello
I have created a system using 1 unit of BQ79631-Q1 and 2 units of BQ79616-Q1. I can display the cell voltages connected via BQ Auto Eval using USB2ANY…
Part Number: BQ79631-Q1 Hello,
The datasheet (SLUSEC2A) mentions that BQ79631-Q1 has a 16-bit third ADC for current sensing (on page 20). However, I have noticed that the current sense ADC resolution is given as 14.9 nV/LSB (24-bit) on page 11 in the electrical…
Part Number: BQ79631-Q1 Hallo!
Is there an errata file for the BQ79631-Q1 chip? What happens if the recommended (-1V to 5V) or max voltage limit is exceeded for the differential voltage measurement (e.g. vc2-vc1 ...)? Does it has an effect on the other…