Hi, I applied 10 s delay, but still, it is not working, I'm trying with only one BQ79656 device.
I'm getting the voltage data perfectly.
I've attached the part of code, please check it once. wakeup_BQ();
init_ASCLIN_UART(); /* Initialize the UART…
Hello Padma,
1. The cell balance can be configured based on the external resistors used in conjunction with the BQ79616-Q1 device up to a maximum of 240mA for 8 cells at ~75C. Please keep in mind that you can only balance odds or evens, so for you…
Part Number: BQ79631-Q1 Tool/software: Hi E2E,
The schematic in the user's guide is in the form of the image, and I cannot search for text within the schematic.
This causes me great inconvenience. Could you please provide the original schematic in…
Part Number: BQ79616-Q1 Other Parts Discussed in Thread: BQ79616 , TXS0102 Hi,
We're designing a system for 32S in which we've stacked two AFE's in daisy chain using capacitive coupling because both AFE's are on the same board.
And also we're using…