Hello David, When going to production, you can use the BQStudio GUI to export what we call the golden image which will contain FW, configurations. The golden image has different output formats which are detailly explained in Section 5 FlashStream® File…
HI, Robin,
If you use USB2ANY, you can use TI online GUI and communicate with USB2ANY.
https://dev.ti.com/gallery/view/BatteryChargers/ticharger_gui/
EV2400 pairs with BQStudio GUI.
Regards,
Tiger
Part Number: BQ76940 Other Parts Discussed in Thread: BQ78350 , BQSTUDIO , , BQ76200 Hi,
I am using BQ78350 and BQ76940 to develop a battery management system, observing bqStudio GUI and having some problems as follows:
1. When FET_EN=0, XCHG and…
Hello Sir,
Yes, Bq Studio is Auto detecting now.
I have observed after pressing the FET_EN command, Noticed Manufacturing Status, Bit 4 become RED. Please check in the sceenshot.after current flowing more than approx 1.15 A for some duration. Bat…
Hi, Robin,
As I previously stated, the BQStudio GUI works with EV2400, it does not support USB2ANY.
On the other hand, TI Charger GUI supports USB2ANY. TI Charger GUI does not need the BQZ file.
https://www.ti.com/tool/TI-CHARGER-GUI
From your…
Part Number: BQ76952 Other Parts Discussed in Thread: BQSTUDIO , , EV2400 Hello team,
I am currently using I2C version of BQ76952 and using EV2400 to configure the BMS IC through the BQSTUDIO GUI.
Can I do the same with SPI Version of BQ76952 using…
Hi Leon,
Yes the fast charge timer in the BQStudio GUI is the charge safety timer.
Leon Shin said: For example if i set REG07 be 00(5hrs), At the end of the 5-hour, the charging is stopped and bit 4,5 of REG0C will be11
This is correct.
Best Regards…
Part Number: BQ78350-R1A Other Parts Discussed in Thread: BQSTUDIO , BQ76200 , BQ76940 , BQ78350-R1 Hi ,
The problem I encountered is that the XCHG and XDSG bits are both high, It makes the CHG FET & DSG FET uncontrollable (The FETs are always turn…
Hi Danilo,
Are you using the EV2400 + BQStudio to communicate with the BQ24773?
The Update Mode is set to "Immediate" by default. This means that any time you change the bits in the BQStudio GUI, these write commands are automatically sent to…