Part Number: BQ4050EVM-561 Other Parts Discussed in Thread: BQSTUDIO , EV2400 , BQ40Z50 hi,
Currently i m working on a BQ4050EVM-561 and communicate to the bqstudio to access the data through SM BUS but the problem is communication is not stable between…
Have you tried communicating a bq25892 official EVM with BQStudio GUI using EV2300 or EV2400? The official bq25892 EVM works for sure. You may compare with your system and try to debug. Thanks!
Hey Jeff,
Is this on the BQ25703AEVM or a custom board?
Does the converter regulate VSYS normally when the input voltage is at 6V?
Do you have a load present on VSYS at the time you apply the 5V input?
Are you using the integrated independent…
Hello Matt,
I restarted the whole setup. FET_EN bit initially is low. After pressing FET_EN, I refresh the list. Bit FET_EN becomes white background momentarily before changing to high. However, bit 6 of Battery Status (DSG) remains high throughout…
Part Number: EV2400 Other Parts Discussed in Thread: BQSTUDIO , BQ4050 , Hello,
As i mentioned in my previous question, I try to work with bq4050 through bqstudio GUI, and EV2400.
Sometimes i loose communication, and the LEDS on the EV2400 turns off…
Part Number: BQ76942EVM Other Parts Discussed in Thread: BQSTUDIO , , EV2400 , BQ76942 Hi TI Team,
I am currently working on a Battery Management System project, using the BQ76942EVM. However, I am stuck with a communication issue when connecting the…
Hey Carolus,
The charger should be programmed to go into OTG mode via I2C and externally, the EN_OTG pin should be pulled high. You will want to verify first that the EN_OTG pin is pulled high on the EVM. Second, verify that the USB controller is actually…
Any I2C adaptor similar to EV2300 or EV2400 may interface with the bq25895 EVM. If user would like to make use of the bqStudio GUI when evaluating bq25895 EVM, EV2300/EV2400 has to be used.
Please refer to https://github.com/tibms/bq2589x for sample…
Hello Vayne,
I would recommend using a separate I2C adapter if you are wanting to script, EV2400 is mainly made for evolution using the TI GUIs.
An example would be using the Aardvark, or a lower cost solution like the USB-ISS adapter.
As Ning mentioned…