Part Number: C6000-CGT Tool/software: Hi Team,
can you share the ECCN number for the following versions of C6000 Code Generation Tools:
C6000 Code Generation Tools 6.1.10
C6000 Code Generation Tools 6.1.13
C6000 Code Generation Tools 7.0.4
C6000 Code…
Part Number: C6000-CGT Tool/software: We are using C:\TI\ccsv5\tools\compiler\c6000_7.4.1 and planning to move to v8.3.1
It is old code base. Will it breakward compatibility?What all things to be considered before making such upgrade,
Part Number: C6000-CGT Tool/software: Compiler: C6000-CGT 8.3.13
This code gets miscompiled if no optimization settings are passed:
e.g. "cl6x.exe enumClass.cpp"
enum class A : unsigned short
{
A1 = 0xFFFFu
};
int test(A a)
{
…
Part Number: C6000-CGT Tool/software: Hello, In the following example, the struct does not contain the expected values after initialization. The 10th element is not correctly initialized. If I use float instead of double for e.g. var5, then the program…
Part Number: C6000-CGT Tool/software: I am looking for the C6000 V8.1 compiler to use with an existing project. The online resources only have version 8.3.1. Is it possible to get a v8.1 download.
Part Number: C6000-CGT Tool/software: The manual says that all v8.3.x versions of the c6000 compiler support C11, but I have the latest version as of today (8.3.13) and I can't select C11. It only goes as high as C99.
Part Number: C6000-CGT Tool/software: Hello,
I encountered some unexpected behavior in one of our products and was able to track the behavior down to an apparent compiler bug. After some trial and error, I was able to work the code into a minimal test…
Part Number: C6000-CGT Tool/software: We are using Code Composer Studio v6.1.3 and attempting to run the XDS 560 Pro Trace emulator. The error is "license cannot be acquired." I have ti_emupack_setup_5.1.636.0.exe which we used in the past but…
Part Number: C6000-CGT
Hi,
I'm facing an issue with dis6x.exe, when I try to run disassembler with a cpp object file it is giving the error as follows:
$ dis6x.exe --all rbRsp_AngleEstimation.cpp.obj
Disassembly of rbRsp_AngleEstimation.cpp.obj: …