Part Number: CC-ANTENNA-DK2 Hello
I would like to integrate the antenna #6 of the CC-ANTENNA-DK2 kit into my design. However, this antenna #6 seems to have one turn less than the helical antenna from the design note DN038.
First: Why is there a difference…
Other Parts Discussed in Thread: CC-ANTENNA-DK2CC-ANTENNA-DK2
I noticed that there are three calibration parts in the design document of TIDC-CC-Antenna-DK2, namely SHORT, LOAD, and OPEN, which are used for VNA test calibration, so its PCB design traces…
Part Number: CC-ANTENNA-DK2 Hi TI team,
On Board#3, supposed to be a dual-band 868MHz-2.4GHz. When I measure the S11 of this board, I get picks at 2.0GHz (and 4.7GHz) which is very far from 2.4GHz, plus there is nothing at 868MHz.
(To be sure, I measured…
Part Number: CC-ANTENNA-DK2
Hi Experts,
I was wondering if I could get dimensions for board number 4 on this TI DK2 antenna kit. I see there are dimensions for the ground plane and the total height, but I don't have the dimensions for any of the antenna…
Part Number: CC-ANTENNA-DK2 Hi all,
I have the CC-Antenna-DK2, and a few launchpads. Both the "quick start guide" and the "antenna measurement summary" documents refer that some antennas can be configured for either 868 or 915MHz, however those whose bandwidth…
Part Number: CC-ANTENNA-DK2 Hi everyone,
I have the CC-Antenna-DK2, and a few launchpads. I want to try antenna diversity but there is absolutely no information about it on the CC-Antenna-DK2 documentation. Two questions:
1 - Is there any guide/tutorial…
Part Number: CC-ANTENNA-DK2 Hey everyone,
The CC-Antenna-DK2 "quick start guide" (and the antenna PCB silkscreen itlself) mentions that antenna #11 has a dual band option for 868MHz and 2.4GHz. However the kit schematic represents the used BOM as the…
Other Parts Discussed in Thread: CC-ANTENNA-DK2 Can anyone able to give me antenna 1 & 3 HFSS design file to understand the design procedure. Thanks to everyone in advance.
Part Number: CC-ANTENNA-DK2 Hi TI experts,
I did a simulation of Board#11 using HFSS (according to the DXF found from https://e2e.ti.com/support/wireless-connectivity/bluetooth/f/bluetooth-forum/630896/cc-antenna-dk-rd-2-4-ghz-pcb-antenna-design-files…