Hi Archit,
Attached the pre-built boot partition which successfully boots to Linux (its a tar.gz file). Please let us know if this works (you may want to run env default -fa and saveenv on the first boot).
Regards
Shravan
boot.tar.gz.txt
Hi Yunus,
We are also facing the same issue.
While inserting g_file_storage.ko it returns error as 'No such device'.
We also get 'musb_init_controller failed' while booting.
I'm suspecting that it would be the issue with interrupt or DMA. I tried…
Part Number: DS90UB953-Q1 Hi Team,
There is a good new that we DIN DS90UB953-Q1
And there have one thing need your support!
Below is customer analog to digital transform module block diagram, customer want to know could 953 receive MIPI from Analog…
I am sorry I missed the explanation. What I was saying: WDT = Watchdog Timer Source: Figure 11-1 CMPSS Module Block Diagram (P.1354) I want to detect overcurrent in software using this module. I would like to use COMPSTS [COMPLLATCH], CTRIPL (to be connected…
Attached are 2 parser preprocessed compiled files. First is the working version. Second is the version that causes an abort (after a few hours of runtime). Below is the copy of the parameters during the build (version is embedded).
"C:/ti/ccsv5/tools…
Other Parts Discussed in Thread: DM3730 , BQ27200 , WL1271 , OMAP3530 , TVP5146 , AM3517 Hi,
I am using DM3730 processor, ov2643 2M pixel camera. when I run the application "VIDIOC_STREAMON: Broken pipe" occurred. After kernel log I attached the C video…
Other Parts Discussed in Thread: CC2538 , MSP430WARE , UNIFLASH , CCSTUDIO I am attempting to install CCS v5 on Windows XP running under VM ware. CCS V4 installed without issue.
I have tried several times including new directory and turning off virus…
Part Number: MSP432E401Y Hello,
We are using the micro controller part# msp432e401y to manage the ethernet switch part# KSZ8863MLL for one of our FANTRAY application.
The block diagram of the FAN Tray controller card has been attached for your reference…
Wojciech,
The attached v0.9.65 installer should have all the required files. I already tried to attach it as an exe, but it was rejected. So, the attached file has its extension changed from exe to txt. Just change it back and run it.
Regards, …