Part Number: CC1020 Hi,
While trying to operate the smartrf studio 6 we got an error message C:\windows\system32\drivers\tvicport.sys
How can I handle it.
Ofer
Part Number: CC1350 Other Parts Discussed in Thread: CC1020 , CC1101 Hi all,
I just start to work on new project that use cc1350 and need to be compatible to old version of this product that use cc1020 with the configuration above:
Device: CC1020…
Part Number: CC1200 Other Parts Discussed in Thread: CC1020 , Hi
I've got a product that's using a cc1020 for wireless communication. Now a new product must be developed that can communicate with the old product. I have no documentation on the old product…
Do you mean how do you know that the programmed datarate and deviation is what you what?
"but the information is different from what I should receive.": Could you elaborate a bit what you mean here?
TX:
CC1020 data sheet: In TX data is clocked into CC1020 on the rising edge of DCLK
AN023: In TX mode, the interrupt should be triggered on the falling edge of DCLK. When the interrupt occurs, write the next bit to be transmitted to the I/O pin.
…
Part Number: CC1020 We have a CC1020 based product that have support for a Manchester coded protocol with a preamble of 0xaaaa. This works fine. Now we want to add support for another protocol that has a preamble of 0x0000. This doesn't work reliably…
Other Parts Discussed in Thread: CC1020 , CC1175 , CC1150 , CC115L , CC1070 , CC1101 Hi,
We want to use the Texas Instruments CC1020 transceiver chip. However, we only want to use it in transmission mode - not receive.
Can you help me with
1)…
Other Parts Discussed in Thread: CC1101 , CC1020 Hi I am trying to get CC1101 and CC1020 to communicate with manchester coding.
When without manchester coding the communication between CC1101 and CC1020 is fine.
But once open manchester coding, it…