Part Number: CC1070 It seems the current version, SmartRF Studio 7, doesn't support the CC1070 - I need SmartRF Studio 6.
So I downloaded & installed Setup_SmartRF_Studio_6.13.1.exe
But when I run it and select CC1070, I get:
This is on Win7…
Other Parts Discussed in Thread: CC1070 , CC1020 Hi All,
I have inherited an RF transmitter project which transmits a device ID as a UART, and I have been asked to develop a receiver to detect and display the ID.
The transmitter hardware is already designed…
Other Parts Discussed in Thread: CC1070 , CC1101 Hi Folks
I have been tasked to investigate the impedance matching on a product of ours, that uses a CC1070 transmitter IC.
I need some information / confirmation on the setup to measure the impedance looking…
Other Parts Discussed in Thread: CC1101 , CC1070 I have both CC1101 and CC1070, and I want a very low power, short range (less than 10 m) transceiver system.
1) If I use CC1101, where can I find reference design and layout for 403MHz (I can find only for…
Other Parts Discussed in Thread: CC1070 , CC1021 Hi
i have e device who use the CC1070 to transmit weather data to a receiver (who use CC1021): 902 to 928 mhz (the device is made for usa) xtal: 14.7-508.
I have the same device (but built for Europe) who…
Other Parts Discussed in Thread: CC1070 , MSP430F249 , CC1020 I am trying to interface the RF chip CC1070 with the MSP430F249 processor.
Is there any helpful information such as sample code, books, web-site, etc
to develop a interfacing code?
Thanks…
Other Parts Discussed in Thread: CC1070 In relation to CC1070 chips we would like to have more detailed
information about certain aspects of CC1070 mentioned below. We would like the designers to kindly comment on these aspects as it will help us in…
It was used due to a legacy cc1070 (chipcon) project. This would be the second project keeping the legacy going.
There were some interesting choices made which makes it hard to follow a payload format.
Preamble - 30 bits (non manchester)
Data - 28 bytes…