Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 Hello E2E community,
I'm encountering an issue with communication between CC1101-Q1 and CC1101 modules, and I'm seeking assistance to troubleshoot and resolve it.
Background: I recently…
Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 , Hi everyone,
I'm working on a project that utilizes the CC1101 transceiver in asynchronous serial mode.
Due to compatibility requirements with existing devices, my client specifies the…
Part Number: CC1101-Q1 Tool/software: Below are two snapshot from the datasheet regarding the data rate,
From Introduction section, it indicates the maximum data rate is 250kBaud,
From the '3.8 Data Rate Programming' section, it states that "The data…
Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 Tool/software: Hello TI Community,
I am currently working on a project involving the CC1101 transceiver, and I need to implement a feature that allows users to set the Carrier Sense Absolute…
Part Number: CC1101-Q1 Hi,
In my application, the user would input a value to specify the carrier frequency they would like to use. And based on this frequency value, I need to configure the related registers in my code.
According to my current understanding…
Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 I configure the GDO1 as the Serial Data Output, that is :
CC1101_Write_Reg(CC1101_IOCFG1, 0x0D );
and then I can detect the signal by a oscilloscope.
With the TX transmission present, the signal…
Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 While the CC1101 datasheet offers circuit design references for individual frequency bands, it lacks reference designs for dual-frequency circuits.
Is there any way to do this ? any suggestions…
Part Number: CC1101-Q1 Tx-If-CCA,
Hi is that setting required for FCC compliance.
I understand that the registers in the application notes may have been using this setting.?
We however would like to potentially develop a Tx only version that once configured…
Part Number: CC1101-Q1 64 IDLE 0 64 OK 65 IDLE 0 65 OK APPEND_STATUS = 1 CRC_EN = 1 66 RX 0 65 - FEC_EN = 0 67 RX 0 65 - 68 RXFIFO_OVERFIEW 1 65 OK
for the cc1101-q1 silicon errata and following setting
Does it mean that for variable packet lenght…