Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 Hi,
I would like to know digital output current number with Logic 0 and Logic 1 for CC1101-Q1.
The number is not found in "2.13 Digital Input/Output DC Characteristics" in CC1101-Q1 datasheet…
Part Number: CC1101-Q1 Hi,
This is about CC1101-Q1 receiver current consumption.
I found below description in CC1101-Q1 datasheet, the current value at 1.2kbps with DEM_DCFILT_OFF=0
I would like to know the current consumption with DEM_DCFILT_OFF=1
…
Part Number: CC1101-Q1 Hi,
How to check if CC1101-Q1 is in SLEEP state or WOR enabled from external MCU via SPI or any other I/F?
Best regards,
-Shibata
Also, Siri, would you mind helping to remind someone who has been assigned to support my earlier post as well?
Here is the link:
CC1101-Q1: Need Help with Noise Reduction and Pulse Width Stability for CC1101-Q1 Transmitter Development in Async mode .
…
Hi Jonard,
Have you come accross that thread: https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz-group/sub-1-ghz/f/sub-1-ghz-forum/1216727/cc1101-q1-cc-debugger-directly-to-a-cc1101-q1-device
As well as figure 10 of that document https://www.ti…
Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 , Hi, I'm looking for a way to connect the CC1101 transceiver to my PC in order to be able to configure it via RF studio software. I cannot afford the cost of an evaluation board since it's…
From the DN022:
" AGCCTRL2.MAGN_TARGET[2:0] is used to set an on-chip target value for the peak signal amplitude. MAGN_TARGET is used by the AGC loop to set the correct gain. "
This means that the MAGN_TARGET setting will affect the RF performance…
Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 , TEST2 Hello, i m using two CC1101_q1 boards which i designed as in application notes of CC1101.
in TX side, put 32 bytes data, wait for the finish of the transmit phase and wait 5 seconds…
Part Number: CC2642R-Q1 Other Parts Discussed in Thread: CC1101 , CC2642R , CC1120 Tool/software: Code Composer Studio Hello
We have a CC1101 SubGig radio connected to a CC2642 via SPI.
However the CC1101 does not use "conventional" SPI; for example:…
Part Number: CC1101-Q1 Other Parts Discussed in Thread: CC1101 Hi! In my situation i have two boards with CC1101 (868Mhz): one for transmit data and one for recieve. The reciever is stationary located and doesn't move. The transmitter moves back and forth…