Part Number: 430BOOST-CC110L Hello, I've bought the Launchpad MSP-EXP430G2ET together with the AIR Boosterpack and tried to connect it to "SmartRf Studio". I've rotated the UART headers. The drivers are: "MSP Application UART1 (COM4…
Part Number: CC110L Hello,
I'm doing a schematic review and I'm noticing that the crystal selected to be used with CC110L is 24MHz and the load capacitance is 6.5pF.
Datasheet specifies 26MHz as minimum working frequency and load capacitance from…
Part Number: CC110L Other Parts Discussed in Thread: TEST2
Hi
I am trying to understand the CCA mode of CC110L. I Have few Queries related to implementation of CC110L CCA mode.
First i will state my register setting related to CCA implementation
…
Part Number: CC110L Hello
I am trying to configure a CC110L transceiver. I configure all the registers and after I read them in order to check the values are correct, and they are.
Then I send the command strobe STX with FS_AUTOCAL=0X01 configured.
The…
Part Number: CC110L Hi,
We have designed an RF beacon using the CC110L device which gives audible 'beeps' on our hand held receiver (an off the shelf item). It has been tested to ETSI EN 300 220-1 and has failed the Adjacent Channel Power test…
Part Number: CC110L Tool/software: Code Composer Studio hello i am working on CC110L and sendin and i has tried to configure cc110l . and i has sent two command to CC110L ,follwing are the command which i has sent to cc110l
#define SMARTRF_SETTING_IOCFG0…
Part Number: CC110L hello,
i am working on project where i am transmitting and receiving data through RF IC CC110L . i want to plot graph of power consumption vs distance .
my question is
1.IC consumption will be same irrespective of distance or will…
Part Number: CC110L Other Parts Discussed in Thread: CC113L , TEST2 Tool/software: Code Composer Studio Hi Sir,
I use CC11xLEM kit and test OOK/no preamble/sync packet format.
The RX still can't receive packet correctly, can you please advise ?…
Part Number: CC110L hello,
i am working CC110L .
i has wrote FIFO in TXFIFO register. when i read back it is showing me what it has tried to read back.
then issue STX command. and i am waiting for STX command to be executed but the strange thing i found…