Part Number: BOOSTXL-CC1120-90 Other Parts Discussed in Thread: CC1120 , CC1125 Hi IT team,
I am trying to use CC1120-90 for a project using another Host controller. but i am not able to set up a stable communication. I tested communication using…
Part Number: CC1120 Tool/software: I am designing in a CC1120RHBR. I need an actual footprint drawing for this part. The datasheet does not contain this information.
This link on the TI site, does not have an actual drawing, it just has a picture of…
Part Number: CC1120 Tool/software: Hi.
I have three different types of PCBA's using the CC1120. I can TX and RX data with each board. The board are configured as such:
Boards 1 and 2: CC1120 with on-board Johanson broadband 868/923 MHz chip antenna…
Part Number: CC1120 Other Parts Discussed in Thread: CC1175 , CC1125 , CC1200 Gentlemen,
We are using the BALF-112X-02D3 balun from STMicroelectronics, but it has become obsolete and cannot be found...
Impossible to find an equivalent, if someone…
Part Number: CC1354P10 Other Parts Discussed in Thread: CC1120 , CC1020 Tool/software: Hello E2E,
I was intended to use radio between CC1354 and CC1120 in 2FSK mode. When I tried to match the SubGig radio packet structure my legacy radio settings need…
Part Number: CC1120 Tool/software:
We are using the CC1120 as a dedicated sub-gig receiver on an IoT device, listening on the 433MHz ISM band. The system register settings are provided below:
cc112xRegisterUpdate_t _regSettingsUnified [] = {
…
Part Number: CC1120 Tool/software: I am designing in the CC1120 into a MURS radio band system operating at 154MHz. The design will use an external power amplifier that will allow for the 2W legal limit for TX power into the antenna.
The system will…
Part Number: CC1120 1. We have a set of CC1120 boards for transmitting and receiving purpose. We transmit the data using 914.070Mhz frequency. We send two Buf values, Buf1 transmit 46 byte data and Buf2 transmit 128 byte data. 2. First step we are not…
Part Number: CC1120 When sending, one of the following errors occurs and the message cannot be sent.
Please tell me the cause and countermeasures.
(1)PLL SETTLING timeout After sending the STX command strobe, the Status Byte STATE[2:0] does not change…
Part Number: CC1120
Hello expertes.
I am a person who is experimenting with the CC1120 in the environment shown in the picture below.
In the last reply, I received an answer that the CC1120 needs to detect the FALLING interrupt on the GPIO2 pin…