Part Number: CC1120DK Hello Guys,
Good day.
The kit seems to be optimized for 868/915 MHz but can the customer make it work in in 865 to 867 Mhz?
Also, the antenna included on the kit is specified to 2dB, can they connect a 12dB antenna to it?
Thanks…
Part Number: CC1120DK Software: SmartRF Studio 2.17.0 clicked on Sub-1 GHz tab.
List of Connected Devices:
TrxEB (USB device ID=2195, Fireware revision=0044), --CC1120
The other TrxEB board does not show up.
Both TrxEB boards are rev 1.7
Both boards…
Part Number: CC1120DK I have bought a new product, CC1120DK(a development kit), but when i get one, the product(LCD) was broken.
I think it was the shipping problem.
I add the photo with the box.
Can you replace the new one as soon as possible?
Part Number: CC1120DK Hi,
I'm looking to buy a CC1120 module with FCC certification.
all vendors can't tell if CC1120 comes with FCC ID.
I Know that these modules exist since I have few of them (see picture below).
please assist me find a vendor…
Part Number: CC1120DK I have two CC1120 dev kits with CC1120 EM which I am trying to connect to SmartRF Studio 7 v2.13.0. The dev kits are powered over USB and I could execute PER and other tests. However, when I launch SmartRF Studio 7, none of the dev…
Part Number: CC1120DK Hello. We have the CC1120DK. We try to test the modules like in the TI video( www.youtube.com/watch , but at the Master I can't run PER STATISTICS and plot the connection because I do not have menu like that. At start, under Main…
Part Number: CC1120DK Dear TI,
I'm using the TRxEB CC1120 version to run some tests and came over some strange behavior.
When I select a preset on SmartRF and modify from there, I get vastly different performance from when I just tweak immediately…
Part Number: CC1120DK Can the CC1120 be configured to transmit or receive a sync signal at a rate of 48KHz? i.e. RF on RF off at a rate of either 48KHZ or 24KHz (and I use both edges). I wish to transmit from 1 x CC1120 and receive on 8x CC1120's. I have…
1) The board has an connector you can use for an external antenna.
2) You can use e2e.ti.com/.../375556 to estimate range.
3) Board #6
4) You can use SmartRF Studio directly with this board (no LP required)
Hi,
I have purchased CC1120DK with 420-470MHz and there is external antenna used in the kit. I found this external antenna is good in performance and I would like to know the supplier and data sheet for this antenna and then try to look for them.
Thanks…