Hi Amrit,
We have checked the continuity and soldeing. It looks fine. Then I have isolated the TPS2640 circuit from the other circuitry and isolated the FLT, SHDN, IMON signals from going to MCU pins. We got the following observation:
Slno.…
The following reference design ( ) how the design could be splitted in a TX and a RX part.
With reference to :
If spliting RX and TX, pin 1 on C181 should be connected to ground. Pin 1 on L193 could be connected directly to the RX port. The TRX…
Part Number: UCC28950 Tool/software: Hi,
There were some calculation inconsistencies with the UCC28950 application note, so I have summarized the calculation results in the document below.
I would like a response to each comment in the Excel file…
Part Number: TPS2663 Tool/software: Hi, in my application, Im trying to connect a TPS2663x to a motor controller board which has 10mF of capacitor on board with 200W max. Using the calculator, I noticed that the device will go into thermal regulation…
Part Number: DRV8300 Hi Team,
Concerns about high temperature of DRV8300 driver Infineon MOSFET IPT015N10N5,only PWM signal, the temperature will reach more than 60C.
Infineon_IPT015N10N5_DataSheet_v02_04_EN-3362538.pdf
Hi,
We have antenna references designs for 169, 433, 868, 915 MHz and 2.4 GHz antennas. https://www.ti.com/tool/CC-ANTENNA-DK-RD
Please see this page for TI energy harvesting solutions: https://www.ti.com/solution/other-energy-harvesting
Regards…