Part Number: CC1120 I have a 434MHZ daughter card that I use on my custom RX and TX boards. In testing with a TRXEB RX board and my custom RX board, I have a TX sending packets from about 3 ft away. Every packet is received every time (in normal mode…
Part Number: CC1120EMK-420-470 Other Parts Discussed in Thread: CC1120 , CC1175 , CC1310 , CC1125 Hi Team,
Our customer is considering the CC1120EM-420-470-RD for nanosatellite application and has some inquiries as follows:
Does the chip CC1120EM-420-470…
Part Number: CC1120EMK-420-470 Other Parts Discussed in Thread: SMARTRFTRXEBK , CC1120 Hi,
I'm looking for hardware design files like schematic, gerber files, PCB layout for the CC1120EMK-420-470 .
And I'm also looking for the schematic of the SMARTRFTRXEBK…
Part Number: CC1120EM-420-470-RD We want to try packet communication between cc1120 and cc1020. First of all, the packet format for cc1020 is unknown. I understand that in order to communicate with the packet, we need to know both the primable and sync…
Part Number: CC1120EM-420-470-RD Dear Sir,
I have two CC1120EM-420-470 (DK) daughter cards, and now I have designed a motherboard to connect it.
But i try to find the CC1120EM-420-470 (DK) daughter card information or documents, they are not show the mechanical…
Part Number: CC1120EM-169-RD Other Parts Discussed in Thread: CC1120 Hello,
I am interested in employing the CC1120 for a 169MHz telemetry application.
Is the 169MHz band legal for use in the USA by the FCC?
Also, does TI make a product for 27MHz?
Thanks…
Part Number: CC1120EM-420-470-RD I've ported code to Arduino UNO and that can run Tx/Rx test successfully.
I would like to porting firmware to STM32G071RB board and run the same initial register setting value as Arduino UNO.
after issue STX command…
Part Number: CC1120EM-420-470-RD
I would like to porting driver to STM32 and found that will block on GPIO2 no response after STX command.
I set "CC112X_SETTLING_CFG = 0x00B" and my partversion is 0x23 no run manual calibration.
my initial…
Part Number: CC1120EM-420-470-RD Hi
I wanted to ask whether there is any way in which I can directly connect a differential input from antenna to cc1120's LNA pins(19 and 20) without using the circuitry involved to convert single ended input to differential…
Part Number: CC1120EM-420-470-RD We have a CC1120 design (433MHz band) on a new product using a helical antenna.
1. Can TI review our design (layout and schematic)? Do you normally do this?
2. Can TI provide any recommendations when using a helical antenna…