Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: BQ34Z100-G1 , BQ76952 , BQ34Z100
Masters of TI,
I met a trouble,
1. My bq34z100-G1 is used with a 52V LFP battery (BMS).
2. The REGIN of bq34z100-G1 is connected to the REG2 (3.3V) of bq76952…
Part Number: BQ34Z100-G1 Other Parts Discussed in Thread: BQ76952 , BQ34Z100 Masters of TI,
I met a trouble,
1. My bq34z100-G1 is used with a 52V LFP battery (BMS).
2. The REGIN of bq34z100-G1 is connected to the REG2 (3.3V) of bq76952 AFE.
3…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: GPCRB Tool/software: We have a project, after low temperature compensation, when verifying the accuracy of low temperature SOC, it is found that FCC will not be updated when the temperature changes…
E030 gg file.gg.xlsx
E030 cycling run 3 Maccor data -increased rest time-.014.xlsx
E030 cycling run 3 Maccor data -increased rest time-.014.xlsx
Hi Wyatt,
Attached is the Cycling data used along side all the smbus information including Gauging…
Thank you for your support. We have modified the discharge test method for testing, which is to discharge at 0.2C for 540s and then stop for 10 minutes and cycle through. However, the test showed: 99%-1% normal, an abnormal jump to 6% at 1%, and then…
Hi
I have attached an excel calculator to help you calculate the impedance of the output ripple. Please use this to check if it matches your design. After that the next thing to consider would be the layout
Regards,
Gerold
Impedance of a Mixed…
Hello Jeff,
Customer has disabled top off timer and result is the same. May we know if you can help to check the attachment for status from customer's board to see if there is anything missing. Thanks a lot!
/cfs-file/__key/communityserver-discussions…
Thank you!
We will check out system in detail again. And If it is nessary, we change Circuit or PCB layout...etc.
And then,
1. How often does do you get a read error? For every 100 readings, how many errors do you get?
>> random. Any board…
Part Number: BQ40Z50 Other Parts Discussed in Thread: BQSTUDIO , GPCCHEM Dear TI partner
How should i get BQ40Z50 chemistry ID;
attachment is my cycle test data at 0 digree celsius.please check,thanks
240017-4-1.xlsx 240017-4-2.xlsx 240017-4-3.xlsx…
Part Number: BQ40Z50-R2 Tool/software: RC decreased from 6662mAh to 6529mAh, RSOC decreased from 100% to 99%.
How to resolve RC and RSOC degradation? Keep a fully charged battery at 100% in relax mode
BT-300_RSOC 100%--99%.xlsx