Part Number: CC115LEM-868-915-RD Other Parts Discussed in Thread: CC115L , CC1120 , CC1101 , TEST2 Hello,
We have a product on hand (whose source code we cannot access) that uses the CC1120 radio, and for one of our commissioned products we've had…
Part Number: CC1125EM-868-915-RD Other Parts Discussed in Thread: CC1125 Can I use SPI data transfer with DMA in cc1125.
As i see SPI with DMA is non blocking call and in cc1125 i need to wait for response to proceed.
Please help ! Is it possible…
Part Number: CC1125EM-868-915-RD Which Mechanism is better -
1. polling or
2. Packet Rx/Tx interrupt based.
In respect with archive high data rate.
Which mechanism used in SmartRF Stdio polling or interrupt.
Part Number: CC1125EM-868-915-RD
i am in rx mode by: trxSpiCmdStrobe(CC112X_SRX);
and now write tx FIFO and submit cmd : trxSpiCmdStrobe(CC112X_STX); -> this is not working
not able to switch from rx to tx, it failed .
Please help.
Does the frequency of 915 MHz and 868 MHz can pass Asia Telecommunications regulations (China, Japan, Korea)?
Do I just setup the frequency range and tx power to meet the regulations?
Part Number: CC1352P Hi,
I understand that OpenThread does not (officially) support 868/915 MHz, while IEEE 802.15.4 does.
From the OpenThread CC1352 Github repository I even see that the example code would throw the error: Platform cc1352 doesn't…
Part Number: CC115LEM-868-915-RD Hi Team,
My customer need to go for FCC certification. And we've two questions need your confirmation:
1) Is our CC115LEM-868-915-RD pass certification? Can we get the certification materials?
2) What's the TX…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 For our project, we chose the STM32 MCU to pair up with separate CC1120s to create a transmitter and a receiver module, instead of using the SmartRf software.
Currently, it seems…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Hi, I am new to using this Transceiver, and I am faced with a problem.
I have paired this transceiver device with an STM32L476RG micro controller, and I am trying to achieve…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Hi!
What is the register configuration for long range mode running at 915MHz?
I want to test the max range of CC1120em in the US.
Thanks.
Joseph