Part Number: CC1125 The low 4 bits of the Status byte are marked as 'Reserved' in the User Manual.
On a read operation, they always seem to be zeros; on write (and Strobe), they always seem to be ones.
Example here: https://e2e.ti.com/support…
I am still not sure I understand what exactly you are trying to do, but there are some misunderstandings regarding how the different registers behave, so I will at least explain them.
When FIFO_CFG register = 0x78 (120), it means that the Threshold for…
Part Number: CC1125 There seems to be some inconsistency in the User Guide, SWRU295E.
In section 3.1.2:
In IDLE state the XOSC and power to the digital core are on
So the digital core is powered-up whenever the chip is in IDLE state
But in section 10…
Part Number: CC1125 Just having questions regards the chip configuration settings?
What happen if we not setting the configuration parameter in the microcontroller setup?
Is that going to set by ZEROs or based on factory setting?
ie: Code snippet below…
Part Number: CC1125 I have successfully implemented a transceiver using CFM and now am starting to implement one using FSK. Before testing, I am carefully checking the status of the CC1125 at each step. I have noticed that the status after flushing either…
Part Number: CC1125 HI All,
how to receive variable size data without predefined length byte (first byte in variable length Pkt mode), because i want to make it compatible with other ic's communication,
CC1125 Has 2 data pkt mode
1. Fixed Pkt mode…
Part Number: CC1125 Hi, I am an FAE Intern and I want to ask a question about the block diagram.
As said, if CC1125 didn't use any IQ signals and upconverting mixers , w hy there was an I and a Q in the functional block diagram?
Thanks!
Part Number: CC1125 Hi, I am an Intern. I have some questions about how to configure registers.
I need to only transmit data using CC1125. So I need to close the preambles, sync, length value and CRC. But when I close the sync by changing SYNC_CFG0.…