I don't know if this was ever resolved or not; but I am having the exact same problem. I just received two new Trxeb eval boards and it wanted to update from 0020 to 0034. After updating, they now no longer show up in the device list.
I'm using the…
Hi Richard!
We have tested the CC1125 With evaluation board development kit but We have a very short range of distance only 0,5km!!! @ 868Mhz and 300bps (2% error rate 100 packets).
The 2 evaluation Kits were in visibility line and about 1 meter…
Other Parts Discussed in Thread: CC1125 Hi all,
I have configured CC1125Cat1 board in Rx mode and is controlled through SPI interface from AT91SAM7S controller. I use CC112x_easy_link as a reference for my coding. Initially i have configured the SPI…
Other Parts Discussed in Thread: CC1175 , CC1070 , CC1020 , CC1125 Team,
I see in the datasheet that it complies with EN 300 220 in low power mode. In High Performance mode, does it comply with EN 300 224 and EN 300 219?
Thanks.
Dear all
I want to program the The MSP430f5348 of the CC1125 from "CCS", when I Run a simple program "interrupt" I get this error message
"No source available for "c_int00_noexit() at 0x5c00" "
Please not that I can excute and run the same code…
If you can, I'd love to have you forward a suggestion to the silicon team working on the cc1120 and cc1125 product families:
I'd like to see future low-power RF products include a way to buffer soft-decision RX data so that users could get higher performance…
I think this may be what you are looking for:
http://www.ti.com/tool/packet-sniffer
It works with quite a few of the dev boards such as:
CC Debugger + SmartRFCCxx10TB SmartRF TrxEB + CC1120|CC1121|CC1125|CC1101|CC110L,CC113L SmartRF05EB + CC2430EM…
Other Parts Discussed in Thread: CC1125 Gents, I do have a mysterious behaviour in some PCB's and we don't find an idea how to tackle: we do have two different designs (form factors), let's call them A (larger) and B (smaller); working in 434MHz transparent…
Other Parts Discussed in Thread: CC1121 , CC1120 , CC1200 , CC1101 , CC1125 I have the CC1120DK with CC1120 and CC1121 radio EMs for testing. We require these radios to operate at 125Kbs in 2FSK mode and 125Kbs in ASK mode. When I am using SmartRFstudio7…
Jackson,
What you are describing above is what is regularly (in Europe at least) referred to as "social alarm". Many companies offer product to support this. Since it is rather important that the RF button works in many (emergency) occasions, European…