Part Number: CC1120EMK-868-915 Other Parts Discussed in Thread: CC1101 , CC1120 Hi.
I am completing a PCB design using this eval board as a reference. I would like to know if all the 47nF capacitors can be replaced with 100nF capacitors on the CC120RHBR…
Hi Zack,
We could move private messaging. I accepted your invitation.
I did not implemented switch to the evaluation board. I just tested 433 MHz and 868/915 MHz separately. After that I implemented 433 MHz matching to our first proto and checked that…
Part Number: SMARTRFTRXEBK Hello E2E Experts,
Good day.
I wanted to buy your CC1175EMK-868-915 product for testing your transmitter. However, the recommended motherboard for this evaluation kit, the SMARTRFTRXEBK, seems to be out of stock in your stores…
Does the frequency of 915 MHz and 868 MHz can pass Asia Telecommunications regulations (China, Japan, Korea)?
Do I just setup the frequency range and tx power to meet the regulations?
The sub-1 PHYs supported can be found in smartrf studio:
For sub1 PHY for 802.15.4, you can also refer to the ti154stack examples:
(in the project's .syscfg file: "RF STACKS" --> "TI 15.4 STACK" --> Radio)
The GFSK PHY…
Part Number: CC1125EM-868-915-RD Other Parts Discussed in Thread: CC1125 Can I use SPI data transfer with DMA in cc1125.
As i see SPI with DMA is non blocking call and in cc1125 i need to wait for response to proceed.
Please help ! Is it possible to use…
Part Number: CC1125EM-868-915-RD Which Mechanism is better -
1. polling or
2. Packet Rx/Tx interrupt based.
In respect with archive high data rate.
Which mechanism used in SmartRF Stdio polling or interrupt.
Part Number: CC1125EM-868-915-RD
i am in rx mode by: trxSpiCmdStrobe(CC112X_SRX);
and now write tx FIFO and submit cmd : trxSpiCmdStrobe(CC112X_STX); -> this is not working
not able to switch from rx to tx, it failed .
Please help.
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Does cc1120 support interleaving and spread spectrum?If CC1120 confirms that these functions are supported, which registers are involved in configuring these functions?
Hello Nir,
I am closing this thread since this is very old and I assume that this issue has been resolved.
Please create new thread if you are still having trouble.
Regards,