Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1190 , CC1120 Tool/software: I am working on a CC1120 + CC1190 custom board with a carrier frequency of 868 MHz , using the following configuration:
Bit rate: 1.2 kbps
RX filter…
Part Number: BOOSTXL-CC1120-90 Other Parts Discussed in Thread: CC1190 , CC1120 , Tool/software: Hi,
I am currently using the CC1120 combined with the CC1190 RF front-end module. The system performs well in open, line-of-sight environments. However…
Part Number: BOOSTXL-CC1120-90 Other Parts Discussed in Thread: CC1120 , CC1190 Tool/software: Hi all,
I'm working on a project using CC1120 in combination with the CC1190 RF front-end module . I need to both transmit and receive data via RF . To control…
Part Number: BOOSTXL-CC1120-90 Other Parts Discussed in Thread: CC1190 , CC1120 Tool/software: Hi, I am using CC1120+CC1190, I need to enable SYNC word configuration and device address configuration to avoid interferences, I configured the device address…
Part Number: BOOSTXL-CC1120-90 Other Parts Discussed in Thread: CC1190 , CC1120 Tool/software: Hi all,
I'm currently working on an RF application using the CC1120 transceiver with the CC1190 range extender (booster pack) , and I need some clarification…
Part Number: BOOSTXL-CC1120-90 Other Parts Discussed in Thread: CC1190 , CC1120 Tool/software: I am working on a CC1120 + CC1190 custom board with a carrier frequency of 868 MHz , using the following configuration:
Bit rate: 1.2 kbps
RX filter bandwidth…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1190 , CC1120 Tool/software: I’m working on an RF application for a weighbridge system. The device’s role is to collect data from load cell sensors and transmit it to a receiver. Device…
Part Number: CC1125EM-868-915-RD Other Parts Discussed in Thread: CC1125 Can I use SPI data transfer with DMA in cc1125.
As i see SPI with DMA is non blocking call and in cc1125 i need to wait for response to proceed.
Please help ! Is it possible…
Part Number: CC1125EM-868-915-RD Which Mechanism is better -
1. polling or
2. Packet Rx/Tx interrupt based.
In respect with archive high data rate.
Which mechanism used in SmartRF Stdio polling or interrupt.
Part Number: CC1125EM-868-915-RD
i am in rx mode by: trxSpiCmdStrobe(CC112X_SRX);
and now write tx FIFO and submit cmd : trxSpiCmdStrobe(CC112X_STX); -> this is not working
not able to switch from rx to tx, it failed .
Please help.