Part Number: CC1125EM-868-915-RD Other Parts Discussed in Thread: CC1125 Can I use SPI data transfer with DMA in cc1125.
As i see SPI with DMA is non blocking call and in cc1125 i need to wait for response to proceed.
Please help ! Is it possible to use…
Part Number: CC1125EM-868-915-RD Which Mechanism is better -
1. polling or
2. Packet Rx/Tx interrupt based.
In respect with archive high data rate.
Which mechanism used in SmartRF Stdio polling or interrupt.
Part Number: CC1125EM-868-915-RD
i am in rx mode by: trxSpiCmdStrobe(CC112X_SRX);
and now write tx FIFO and submit cmd : trxSpiCmdStrobe(CC112X_STX); -> this is not working
not able to switch from rx to tx, it failed .
Please help.
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Does cc1120 support interleaving and spread spectrum?If CC1120 confirms that these functions are supported, which registers are involved in configuring these functions?
Hello Nir,
I am closing this thread since this is very old and I assume that this issue has been resolved.
Please create new thread if you are still having trouble.
Regards,
Part Number: CC120XEM-868-930-RD Hi All,
The customer is asking questions about Post's comments below.
The figure below is a circuit diagram of the antenna part of CC1125EM_Cat1_schematic.pdf in the article.
1. Is it correct to replace part A…
Part Number: CC1120EM-868-915-RD Hi. I am using cadstar design viewer to look at the design files for the EVM. I am interested in the layout for reference/ But for the .pcb file, I am only able to view the placement. I am not able to see any layers or…
Part Number: CC1120EM-868-915-RD Other Parts Discussed in Thread: CC1120 Is there any effect in functionality with Perl scripts for module that is FCC approved compared to those who did not FCC approved ?
Part Number: CC115LEM-868-915-RD Hello,
We have a product on hand (whose source code we cannot access) that uses the CC1120 radio, and for one of our commissioned products we've had to adapt these radio settings to the CC115L, which we're also using…
Part Number: CC120XEM-868-930-RD My customer who develops the wireless board using the CC1200 has tried to look into our reference design , would also like to add the LNA and the SAW filter into their own board.
1. Customer would like to add an LNA to…