Part Number: CC113L Other Parts Discussed in Thread: CC1120 The data sheet states that the minimum data rate for the device is 600bps with a 26Mhz crystal
is it possible to set a data rate at 500bos with a different crystal.
we are using 2-FSK. I don't…
Part Number: CC113L
Hi there,
I have a question about the frequency offset compensation behavior after the auto calibration done.
According to the CC113L datasheet, when FOCCFG.FOC_BC_CS_GATE=1 is set and the receiver is in no signal condition (the CS…
Part Number: CC113L Other Parts Discussed in Thread: CC115L , team,
from field:
Is it possible to add some sort of addressing to the packages?
Is it possible to have a single design that can be used in the frequency bands used in the US and in Europe? …
I have not found anywhere in the CC113L data sheet where it says that the preamble needs to be sequence of alternating bits to be able to receive.
The datasheet says the following:
"The preamble pattern is an alternating sequence of ones and zeros that…
Part Number: CC113L I use the MAX7044 OOK modulation 433MHz as transimitter. Could I set the CC113L as Normal Packet mode to receive data from the MAX7044 OOK 433MHz transimitter? If it is possible, how to implement? How to send the code from the MAX7044…
Part Number: CC115L Other Parts Discussed in Thread: CC113L , CC1101 , CC1310 Hi,
is CC115L and CC113L part numbers can set up in transparent mode? we are looking some alternative that work as transparent mode.
Thank you in advance
Kind regards
Stanesl…
Part Number: CC113L Other Parts Discussed in Thread: CC115L , , CC1310 Dear TI Experts,
My customer is designing a wirelss microphone project which will work at 470~510M band, they want to know if CC113L&CC115L are suitable for this application.
Could…
Part Number: CC113L Other Parts Discussed in Thread: CC1200 , Hi
I send a data packet from cc1200 evaluation borad and receive that data in ook modulation without manchester codding.
But when i send that data with the same frequency and symbol rate in manchester…