Part Number: CC115L Other Parts Discussed in Thread: CC1101 i try to set the chip to -6dBm at 314MHZ/250kbps, the smartRF studio shows that "Valid values for TX power, Highest TX power with ramping: 10 dBm". is is possiable to set the chip to -6dBm at…
Part Number: CC115L Other Parts Discussed in Thread: TEST2 Hi!
I am trying to transmit some data from my stm32, but no transmission is detected. All settings and PA_TABLE values are exported from the RF Studio, except IOCFG2=0x45;
static const registerSetting_t…
Part Number: CC115L Other Parts Discussed in Thread: CC1101 Dear TI E2E Team,
I am not getting proper data by transmitter.
I followed these steps.
1. CS=LOW, Initialize the register in brust mode, Not used register written = 0x00,
reserved and register…
Hello,
I would like to verify that I understand the CC115L datasheet correct.
On page 38 under "Table 5-12. GDOx Signal Selection (x = 0, 1, or 2)" in last row:
"(0x2F) HW to 0 (HW1 achieved by setting GDOx_INV=1). Can be used to control an…
Other Parts Discussed in Thread: CC115L , CC110L , TEST2 Hello,
We are using the CC115L without any interrupts driven. When tested upon power-up the GDO0 and GDO2 are active for a few uSec.
What should be done for production?
Should we terminate the Pin…
Other Parts Discussed in Thread: CC115L , CC1101 Hi, I am trying to implement pocsag protocol using CC115L to connect to pager (apollo AL-901L). In SmartRF studio I set
Base frequency = 432.999817 MHz,
Deviation: 4.760742 kHz,
Data rate = 2.39897 kBaud …
Other Parts Discussed in Thread: CC115L Hi,
a customer of mine struggles with current consumption of CC115L at final production test. Is it possible that the environment at the production test site influences e.g. the radio PA such that a current consumption…
Other Parts Discussed in Thread: CC115L Hi,
We have a design based on CC115L which creates some type of RF interference in frequencies above the main carrier.
This interference is seen only when we transmit above -15dBm, when we use lower power it disappears…
Other Parts Discussed in Thread: CC115L Hi,
I want use MCU to confige CC115L to send unmodeled wave ,and use it to measure TX power. I don't know exactly what's the procedure to do it.
I have successful use CC115L to send modulated data ,but i don…
Other Parts Discussed in Thread: CC115L Hi everyone,
I want to know the behavior of CC115L.
When this device has clock failed during IDLE state, is there a possibility that the current flows from XOSC_Q2 pin?
For example, when XOSC_Q2 is short to GND,…