Part Number: CC1200 Tool/software: Hello:
The customer has a project that requires C1200 chips and needs to refer to the schematic diagram,Please help provide,Thanks!!!
翻译
搜索
复制
Part Number: CC1200 Other Parts Discussed in Thread: CC1190 Tool/software: Hello, we are currently planning to design a board using CC1200 and an external PA. Right now we have a few questions:
When connecting the PA output to the antenna and LNA pins…
Part Number: CC1200
Tool/software:
The above linked post is over a year old with no replies. I'm refreshing the questions in hopes of a response.
1. Regarding format A (2 byte sync, no preamble gating), are there register settings that will allow…
Part Number: CC1200 Tool/software: Hi team,
Can we use CC1200 on frequencies that are not those specified in the data sheet, between 160 MHz and 280 MHz at fixed frequency ?
What is needed to set up a preliminary test system and what demo boards…
Part Number: CC1200 Tool/software:
Hello,
I have some questions regarding the CC1200 at 868MHz:
In the CC1200 datasheet, Table 4.1 shows that the maximum voltage on the analog pin is 2V. However, when we supply 3.3V as per application note (SWRR121…
Part Number: CC1200 Tool/software: We are using CC1200 module, configured at 916MHz. As part of our testing, the PCBs with proper enclosure go through a thermal cycling test to verify any board level issue:
1. -35 to +55 degree Celsius with (3-degree…
Part Number: CC1200 Other Parts Discussed in Thread: CC1260 Could you please advise the status of Part # CC1260RGZR, it was earlier not found on website but 'Active' now.
Thank you in advance for your help!
Part Number: CC1200 Hi,
I have a scenario, where I want cc1200 to only be in reception mode and receive all the packets in air, much like smart RF. I have the same register settings as smart RF.
But, in certain cases where the interval between consecutive…
Part Number: CC1200 Hi all, the programming guide for CC1200 gives the symbol rate register definitions as shown.
However, the equations don't seem to check out; with the default SRATE_E value of 4 and the default SRATE_M value of 239914, the symbol rate…