Part Number: CC1200 Hello,
Measuring TX time of 2-FSK packets of various lengths at a 20K rate using CC1200-EMK by monitoring GPIO MARC_2PIN_STATUS[0]. The measured TX duration is longer than my calculations show. For example, implementing standard packet…
Part Number: CC1200 We have a requirement where we have to reduce the RF current consumption.
From the Ref. Manual , SWRA428 and the excel sheet provided along with, we understood that in packet mode, with preamble size 30, the least we can reduce current…
Part Number: CC1200 I am experiencing problems with using the AES128 module in the CC1200.
I have followed the sample codes previously posted and app note (SWRA483), example 2.
After I execute the TX FIFO encryption code steps 1-11 (P6 OF SWRA483) , all…
Part Number: CC1200 Other Parts Discussed in Thread: CC1190 , In the user manual in all the places where RSSI offset is mentioned, the offset is considered to be -81dBm. Is that a constant value to be used? or it has to found out with experiments according…
Part Number: CC1200 Hello,
It looks like "Saving Configuration" and "Open Configuration" features for the Smart RF Studio 7 v.2.28.0 (build #364) for CC1200 doesn't work. When I have saved configuration of my project and opened it, all setting are different…
Part Number: CC1200 Hi, My customer is using CC1200 with GFSK 100kbps. He wants to improve sensitivity and wonders DSSS PN mode can be used. According to User's guide (SWRU346B) section 5.2.5 "DSSS PN Mode", the mode can be enabled by setting MODCFG_DEV_E…
Part Number: CC1200 We are not Getting actual sensitivity. After -96 to -100.we are doing 500 Packet Testing but we are receiving only less than 100 ACK Packets
Part Number: CC1200 Other Parts Discussed in Thread: CC1101 , , CC2500 , CC1100 Hi, the CC1101 includes WOR and the CC1200 eWOR. Is there a difference?
Regards, Holger
Part Number: CC1200 Other Parts Discussed in Thread: TMS570LS1114 , TI Hercules TMS570LS1114 and RF Transceiver CC1200.
I have developed a working Radio system using a Master and multiple Slave arrangements, utilising a TDM architecture so timing is critical…
Part Number: CC1200 I want to set CS Threshold register to implement EWOR with RX termination on CS.
But when I apply a known signal strength, I read RSSI with some deviation because of which I have set the AGC_GAIN_ADJUST register as 0xB0.
I want to set…