Part Number: CC1201 in the ds, the cc1201 support 4gfsk 1.25Mbps;
If i donot use the internal protocol, we use 8fsk or 16fsk in transparent transmission mode , the data rate of cc1201 can support 4mbps?
Part Number: CC1201 Dear
In the specs. there is a capacitor of 0.9p connecting to the antenna.
The admitance of this capacitor at 400MHz is more than 400 ohm.
This seems to be very low value pf capacitor.
What is the reason to this value?
Part Number: CC1201
Hi.
I am trying to use the CC1201 to retrieve angle samples from the CORDIC at a data rate of 100 kHz. However, the RX bandwidth is 833.33kHz (direct down-conversion), which means that the ADC sample rate and CORDIC update rate…
Part Number: CC1201 hello all,
we want to use the cc1201 Transparent and Synchronous Serial Operation, would you please give some examples?
thanks for your reply.
We suspect that it might be due to the stringent rise/fall time of 2ns the CC1201 requires for CMOS TCXO, and probably the clock in use does not achieve that. I was able to connect a 40MHz clock out of a clock buffer (high driving strength) and the CC1201…
Part Number: CC1201 Other Parts Discussed in Thread: CC1200 , CC1310 Does the 1201 require any delay between bytes when writing to the TXFIFO?
I am running the SPI at 6MHz - if there is a delay between bytes as high as 2uS - then the write is successful…
Part Number: CC1201 Other Parts Discussed in Thread: CC1350 , , CC1310
I am looking for a product with the following specifications.
===========================================
BLE: supported
WIFi:supported
Sub 1G:supported
Frequency:358.5000MHz…
Part Number: CC1201
Hi,
we would like to use the CC1201 transceiver on our application but before we buy the evalutionboards i have a few questions:
Does CC1201 also works on 13MHz/27MHz/40MHz? I would like to use it on the low ISM Band frequencies…