Part Number: CC1310 Tool/software: Hi there!
Set up info:
CC1310F32 microcontroller
NoRTOS application
RF Single Mode
Proprietary RX and TX
SDK 4.20.02.07
CCS 12.8.1
I want to find out if there could be an RFQeue buffer overflow under rare / unusual…
Part Number: CC1310 Tool/software: Everyone,
I’m currently working on a project using the CC1310 platform and need to implement a Wireless M-Bus (EN 13757-4) communication link. However, I’d prefer not to license the third-party stack from…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Tool/software: I'm having problem remapping the IOs in CC1310 resource explorer examples on Launchpad.
Example is:
i2ctmp_CC1310_LAUNCHXL_tirtos_ccs
in the CC1310_LAUNCHXL.h file…
Part Number: CC1310 Tool/software: Hello there,
Currently I am checking out the CC1310 wireless microcontroller. The plan is to use this chip as a UART wireless interface, and I want to use the differential output with external bias. I know I could copy…
Part Number: CC1310 Tool/software: Operating modes UART?
I have interfaced a sensor with LoRa to my UART bus on CC1310. When I send a command to the sensor it responds “+OK” indicating that the command was successful. When I sent the command requesting…
Part Number: CC1310 Tool/software: Hi,
how can I get memory map / allocation in new CCS (Windows 10, CCS 20.1.0.6__1.7.0) .
I get message " The project must be successfully built first. " even if project is build and run on board, in this window I…