Part Number: CC1311P3
Hello,
Can the CC1311P3 provide +20 dBm conducted TX power at 433.92 MHz or within 400–500 MHz?
The datasheet specifies approximately +13 dBm at 433.92 MHz, while +20 dBm is specified at 915 MHz. Can the TX_20DBM_P/N high-power…
Part Number: CC1311P3 We are evaluating the CC1311P3 for a 25 kHz narrowband 2-FSK system with the following approximate configuration:
Modulation: 2-FSK
Symbol Rate: 19.2 kbps
Modulation Index: ~0.45 to 0.5
Frequency Deviation: ~4.3 kHz
Channel…
Part Number: CC1311P3 We have a setup with the following RF configuration on CC1311P3:
Modulation : 2-FSK
Frequency separation(deviation): ±2 kHz (4 kHz total)
Baud rate : 19.2 kbps
Modulation index : 0.208
Rx filter bandwidth: 24.5/29.4KHZ…
Part Number: CC1311P3 We are working with the CC1311P3 device in proprietary RF mode and observing a frequency error when operating above 430 MHz. And, we are using a custom CMD_PROP_RADIO_DIV_SETUP_PA configuration with overrides specifically for operation…
Part Number: CC1311P3 Tool/software: Hi,
Try to add rssi to received packet, set
. rxConf . bAppendRssi = 0x1 ,
and increased
NUM_APPENDED_BYTES
but cant find resonable looked data of rssi. Value are from -33 to 99.
Frame I looked…
Part Number: CC1311P3 Other Parts Discussed in Thread: UNIFLASH
Hi,
I undone CPU DAP and PWRPROF TAP for security reason. After flashing cc1311p3 works as expected.
I try forced flash erase from flash programmer 2 but I got
Enumeration failed…
Part Number: CC1311P3 Tool/software: Hi,
When wakeup from
Power_sleep (PowerCC26XX_STANDBY); by GPIO.
Do I need to init UART from beginning? or in other way? Do I need restart thread with uart read/write loop?
Regards
Marek
Part Number: CC1311P3 Tool/software: Hi,
Could you recommend example with power sleep/standby (to limit power consumption), with RAM retained and wake-up to full throttle.
Regads
Marek
Part Number: CC1311P3 Other Parts Discussed in Thread: SYSCONFIG I am working with CC1311P3 and observing a crash when enabling RF Temperature Compensation in SysConfig.
Issue Description
When I enable RF Temperature Compensation in SysConfig and…