Part Number: CC1312R Hello,
This link in the SDK documentation for the 15.4 API guide is broken:
https://software-dl.ti.com/simplelink/esd/simplelink_cc13xx_cc26xx_sdk/7.40.00.77/exports/docs/ti154stack/mac_api/html/index.html
Referenced from the 15.4…
Part Number: CC1312R Hi team,
After importing the simplelink_cc13x2_26x2_sdk_4_30_00_54 into CCS and without making any modifications to the example, an error is encountered upon attempting to build the project:
"Cannot build project. Referenced RTSC…
Part Number: CC1312R Other Parts Discussed in Thread: SYSCONFIG , CC1310 Hi guys:
I used the cc1312 15.4 protocol stack. Previously, I used cc1310, but the flash and RAM were not sufficient to support our business. Therefore, we recommended cc1312 based…
Part Number: CC1312R Hi Team,
I want to use ADC to sample mic, and then modify the sampling source through ADCbuf in the SDK example.
Please tell me where to modify the sampling source of ADCbuf in the SDK example.
Did you modify the sampling source…
Hi sid:
AON_PMCTL_RESETCTL_SYSRESET_BITN)=1;
There will still be situations where the restart fails. Can you help me find a solution to this restart problem again?
Regards,
faker
Part Number: CC1312R Other Parts Discussed in Thread: CC1310 Hi,
I asked a similar question for CC1310 and SDK v4.x based network, back then the limiting factor seems to be flash and RAM on collector nodes. In CC1312R, both flash and RAM are considerably…
Part Number: CC1312R Hi guys:
I am using the latest SDK from CC1312 15.4
I use Queue. h and use its routine code, as shown in the figure:
This example code is not a problem, but my requirement is to store a batch of data in this queue during startup…
Part Number: CC1312R Hi guys:
I am using the 15.4 protocol stack, collector, and sensor_oad_offchip example project, with SDK version 7.10.02.23
Our project is undergoing final testing.
When testing the load function
The collector issued a packet, and…
Part Number: CC1312R Other Parts Discussed in Thread: Z-STACK , SYSCONFIG Hi,
According to previous posts on this forum and also notes in syscfg file, we can increase the number of Max Devices up to 150 from the default number 50. I have to two questions…
Part Number: CC1312R Hello all,
In my design I want to have an OAD image in the external flash as well as a backup factory image.
My OAD flash sector is 0x80000 bytes in size, from testing I saw that both factory image and OAD image can't fit into this…